Hi,
we would like to sync two 28075 and their PWMs via external sync.
Sync output from one controller can be done via OUTPUTXBAR.
Sync input on the other controller is unclear:
EPWMSYNCINSEL in the reference manual spruhm9d.pdf (13.14.2.3) has no real explanation, only "+I722"
In Figure 13-49, EXTSYNCIN1/2 are connected to Input X-Bar Input5/6.
In Table 13-130, I can select EXTSYNCIN1/2 for EPWM4SYNCIN, EPWM7SYNCIN, EPWM10SYNCIN.
How can I select external sync for PWM1 (shown in Figure 15-8)?
What is the meaning of the EPWMSYNCINSEL bits?
Thanks in advance,
Stephan