Part Number: TMS320F28377S
Other Parts Discussed in Thread: CONTROLSUITE, C2000WARE
Tool/software: Code Composer Studio
Hello team,
Hope you are well. Please see below question from the customer:
We’re using a TMS320F28377S for an application and have some questions about TI’s example code software.
We started our project using the BOOSTXL_BUCKCONV project (Buck_VMC_F2837xS) which got us started, and we imported that through controlSUITE.
We now want to add CAN functionality, and discovered through C2000Ware the can_ex3_external_transmit program which has some example code to get started.
What is the best way to bring that library into the original project using CCSv7.3?
After trying a few times to combine them, it looks like the underlying drivers/dependencies for either are two separate code bases and there are different linker files, clock initialization routines, etc
Regards,
Randhir