Hi,
We have developed our own inverter based on the design in the DRV-69M-KIT. Now we have an issue with the driver.
When running the ID-process with lab2c we get good values and everything goes well. Motor spins up and valueas are repeatable and very similar to that from the KIT. However, if we now reenable the RUN command we just get an erratic jumping around motor with our driver(not the kit) and sometimes a complete driver failure. (We have 10 pcbs that all reproduce these results.)
We are really trying to identify the problem here. We have made huge efforts on the pcbs, with solid 5oz copper and kelvin connections to the three current sensing resistors connected(0.002Ohm) The trace lenghts are also very short, no single one more than 2 inches.
Anyone have an idea what could be the issue? We think since the identification is all well, this should work. Any ideas also what we could measure, change or anything. We are pretty desperate at this moment.
Would it be beneficial to double the current sensing resistor to enhance sensitivity? (And of course adjust current scaling accordingly.)
I am certain there is an issue with either the voltage feedback cirquit or current feedback. Which one is used during the ID process?
Could it be noise from oversaturated gates on the mosfets? We shall try with higher resistance on the driver gates.
Any input is highly appreciated!
Br,
Mikael