This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28377S: New project - simple port set

Part Number: TMS320F28377S

Tool/software: Code Composer Studio

Hello,

I just getting started with texas mcu. I create new project and i wrote simple porgram, like this:

void main(void)

{

EALLOW;

GpioDataRegs.GPASET.bit.GPIO2= 1;
GpioCtrlRegs.GPADIR.bit.GPIO2= 1;

while(1);

}

Offcourse this program doesn`t work. But when i copy this program to example project blinky_cpu01 a have on GPIO2 3.27V. All another lines in blinky _cpu01 project are comment and i include the same files. What and where i must set in new project to run this code?

I am waiting for a response...