This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28M35H52C: 12 GPIO configuration as external interrupt

Part Number: F28M35H52C

Hello,

i have gone through external interrupt example of concerto C2x core. This example shows 1 external interrupt is assigned to XINT1 and another to XINT2 . 

But i have to use 12 interrupt signals on C2x core. As per manual there are only 3 external interrupts are available i.e. XINT1, 2,3 .

So how can i divide and assign my 12 input interrupt signals in group of 4 to these 3 external interrupts.

also is there any connection between m3 core and c2x core for doing this.

Regards,
Sandeep