Other Parts Discussed in Thread: TMDSADAP180TO100, CONTROLSUITE
Hello,
I am working on concerto control card, on which i am using PWM4. for that i have written code in which PWM4A output is mapped on PA6 pin and PWM4B output is mapped on PA7 pin.
Out of these two pins i am getting proper pwm frequency signals on only PA7 pin and PA6 pin remains low. Not getting the reason why it remains low..
After that i configured PA6 and PA7 as GPIO output and toggled both pins. But in this situation also PA6 remains low, PA7 is toggled properly.
So my question is whether this particular pin is used for something else on control card, or is it available as it on 100mm Docking station.
Regards,
Sandeep