Part Number: TMS320F28069M
Hi,
I've had two years now with making InstaSPIN enabled products, all in the ~1 KW / 310 VDC category, many great success stories.. Also many vaporized MOSFETS :)
We are specifying a prototype now that needs to control two 50 KW BLDC's in a vehicle and provide some higher level control algorithms such as implementing a normal mechanical differential in software.
I am thinking building a sample based on Lab12c (Dual motor Sensored Velocity Control) and I have the following questions:
1. Is InstaSPIN-MOTION most suited for an EV type application (i.e. Throttle Input -> Velocity Setpoint?)
2. Is there any application notes for using remote Hall current sensors or any specific types of encoders / resolvers that have been proven to work well?
3. With sensored operation, do we still require the same Motor ID process (Rs, L) as when using FOC?
Thanks
Stomp!