Hello, I am using TI F28069 ControlCARD with a third party DSP hardware. The DSP board has a level shift circuit with a 16‐bit dual supply translating transceiver IC 74ALVC164245 with the help of which it is converting 0 to 3.3 V PWM to 0-5 V PWM signals for IGBT gate drivers. However, I am using SKYPER 32 PRO R gate driver board (as per below datasheet pdf link). I would like to know if there is a suitable level shifter that can be used to give PWM signals to these drivers? The drivers are going to switch the modules for driving the 3 phase motor. Also, should I use something like optocouple for isolation in this case for level shifting from DSP board to driver board?