Part Number: TMS320F28054M
I have a custom f28054m board for motor control. Things are working fine, however during startup, the motor sometimes wobbles little back and forth a bit (2 to 3 degrees) before starting normally. I observed on CRO and found out that when wobbling occures, the three phase current passing through motor reaches motors rated current. I am therefor suspecting that if motor rotor doesn't latch up with current vector at startup, this condition occurs - Is there a way to overcome/minimize this.
Points:
1. Is related to motor tuning especially speed loop tuning parameters?
2. Is this related to motor acceleration?
(Practically I found no specific relation)
is it possible to fine tune motor starup (force angle?) by adjusting parameters like
#define USER_ZEROSPEEDLIMIT or
#define USER_FORCE_ANGLE_FREQ_Hz
Any other guideline to fine tune motor starup against heavy (30times motor inertia) and rated torque? The motor runs on analog input and minimum speed allowed is 100rpm