Part Number: TMS320F28069
Other Parts Discussed in Thread: AFE031
good afternoon to every one,
I'm trying to build a small PLC network using the TMS320 + AFE031. I got the development kit and the attached "G3 Host Message protocol specification" but there are a lot of "black holes".
In principle I don't need the full G3 stack, my idea was to just transfer data over the PLC, implementing my own protocol on top of the basic "data transfer messages".
The problem are:
1. it is not clear what the different "device modes" mean, i.e. if one of them can suit my needs.
2. in the DATA_TRANSFER section it states for G3 normal data transfer a standard IPv6 data packet must be used as a payload, while in lower MAC mode it is not clear what the HCT Connection Handle is
Can someone help me in clarify all these points?
thanks in advance