Other Parts Discussed in Thread: CONTROLSUITE, C2000WARE
Tool/software: TI C/C++ Compiler
Hi,
Need suggestion. I have loaded the USB programs given in the ControlSuite to the target board. The board is developed in our own design. I have checked the hardware.
VBUS is connected to GPIO46 through 100K Resistor
D+ and D- are connected to GPIO42 and GPIO43
Ground is also matched.
When i load the code, the Device manager shows that "Unknown Device". I don't know how to check the output. I am using usb_dev_bulk example. How to give the input?
Regards
Shirly Chrisia. D