Part Number: LAUNCHXL-F28069M
Other Parts Discussed in Thread: BOOSTXL-DRV8305EVM, TIDA-00774
Tool/software: Code Composer Studio
I uses the Launchpad-28069M and the BoostXL-DRV8305EVM to evaluate the InstaSPIN-FOC.
and now I wants to use this solution to drive my BLDC.but I have some questions about instaSPIN application.
Please give me a hand ,thanks.
1.BoostXL-DRV8305EVM parameters :
Supports 4.4- to 45-V voltage supply and up to 15-A RMS (20-A peak) drive current.
15A RMS and 20A peak motor winding current, According to the sampling resistance of 0.007, the amp gain is 10 , so 1.65 / (0.007 * 10) = 23.57 A
it is basically matches the 20A .
but, How much the bus current can be avaliable under 24V dc bus ?
the dc Bus current and winding RMS current, the winding peak current have no math relationship?
Is this related to Trapezoidal wave control and sine wave control?
2. The above problem is mainly due to my application of InstaSPIN . my motor parameters as shown below:
and I just know the max DC bus current ,max Power(W) and the rated voltage of my motor.
I do not know the RMS and Peak wind current .
So,I do not know how to slect the value of shunt resistance.
2.This is a motor drive test parameter at TIdesign. Analyze the following parameters, the dc bus current is larger than the RMS winding current. Is this true for all motors?
Now I just want to know how to design my current sampling circuit when I only know the motor power, voltage and bus current. and select the sampling resistance value?
Thanks.