Part Number: LAUNCHXL-F28027
Other Parts Discussed in Thread: TMDSDOCK28035
I am looking for a Microcontroller unit that is designed for power electronics. We are building a boost and/or cuk converter and this MCU needs to send PWM out to a gate driver to control the duty cycle of a IGBT or similar silicon carbide power transistor. I am considering the C2000 Piccolo MCU F28027 LaunchPad Development Kit however I want to verify this is a good kit for this application. If there are suggestions from TI that would be greatly appreciated. If there was a kit with a gate driver onboard then that might be best however please include a suggestion for a gate driver if possible. This converter would be for a PV system that is roughly 1.2kW to 1.5kW in size. Max voltage from the PV cells is roughly 100 volts, with the converter output at 300 to 400 volts DC. Thank you for your help.