This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28335: epwm TBPRD setting problem

Part Number: TMS320F28335


Tool/software: Code Composer Studio

Hello Sir:


I have met a question related to TBPRD setting;


Refer to manual :


frequence = 1/ ( (TBPRD + 1) x TBCLK))

frequence means the frequence that I want to set (150KHz) ; and TBCLK fixed to 100MHz


so :


TBPRD = TBCLK/frequence - 1;


TBPRD = 100000000/150000 - 1;


TBPRD = 666.6666;(Can't be divided exactly byTBCLK )


because TBPRD is integer,so TBPRD set to 666;


The question is : if I set TBPRD to 666; and run 1second , it will send 150150 pluses , but in theroy , I want to  send 150000 pluses ;


So is there any method to slove this problem?


Thanks!