Part Number: TMS320F28069
Other Parts Discussed in Thread: C2000WARE
Hello,
I am building a circuit that controls the pre-charge of the capacitor. The circuit basically closes a pre-charge relay for first 3 seconds enabling pre-charge and after 3 seconds, it open this signal and powers the contactor relay for high current to flow through cap directly. I want to know if I can use any digital micro controller that identifies a fault (by checking voltage drop at 3 seconds to be within required range) and if there is a fault, it should communicate with F28069 DSP and stop the program. If there is no fault, the logic board with F28069 can start working (enabled). Can this communication between the microcontroller 1 (precharge circuit) and F28069 happen through SPI? I would appreciate if you can also provide any link or document that talks about this kind of information (interfacing the two micro controllers).
Thanks