This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335: Send data to AD5344 by xintf

Part Number: TMS320F28335


Hi, I have an evaluation circuit board on which TMS320F28335 and a Digital-to-Analog chip - AD5344  are connected with each other by xintf.  Which block should I choose to fulfill this function? I have the external addresses of AD5344, which one of them is 0B0000H, and this address is located in xintf zone 6. should I use the block "Memory Copy"? I have tried it, but the generated code correspond to this block is automatically assigned in the "Model Initialize  Function", which  is executed only once.  I want to send data to AD5344 by xintf during whole the process. How  can I do it?

I use ccs6.1 and matlab 2017a on my computer, and XDS200 emulator.

Best regards

K.K