Part Number: LAUNCHXL-F28069M
I recently ported a custom 28069-based instrument to the LaunchXL-F28069M, just as an experiment. Development was easy, but my clients are complaining that they can't see the COM port unless they install CCS, which they'd prefer not to do. (The instrument communicates to a PC over a VCP on the B side of the XDS100.) I can talk to the COM port because I installed the drivers when I installed CCS, but I don't expect my clients to have to do that. On the previous instrument, I used the FT230 USB interface, which installs automatically on modern Windows PCs. So what I need is either some way to hack the .ept file of the FT2232 to make it look like a generic part that doesn't need TI software, or the simplest-possible path for my clients to install the necessary drivers. Any thoughts?