This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am trying to drive an ACIM using lab12b using my own hardware. Motor nominal current is 11A.
I load the motor with nominal load and driving it with a scalar control(V/f control) device. Then at rated speed I measure phase current as 11Arms.
But with my hardware and using lab12b with the same load I can reach up to %95 of rated speed with 12Arms phase current. I see that if I decrease USER_MOTOR_MAGNETIZING_CURRENT I cannot provide enough torque and motor draws so much current like 40-45 Arms. If I increase USER_MOTOR_MAGNETIZING_CURRENT value, the current decreases but the motor cannot reach final speed.
Moreover do you think that a wrong value of USER_MOTOR_RATED_FLUX can lead such a situation? If I put a higher value to that parameter, can it limit the speed?
What do you recommend me to do for solving this problem?