Part Number: TMS320C28346
Hello,
I have an existing Design with the TMS320F28346. During a Review we found an issue with the clock input.
We are running the unit with an external 25MHz clock at XCLKIN input. The datasheet requirement for the rise/fall Time (Chapte 6.8 No. C9,C10) is 4ns maximum.
Actually our actual design gets only 6ns at that pin. Is it possible to run the controller with the reduced rise/fall time?
We actually don't see any problems there, and quarz oszillators with 25MHz/4ns are very rare and hard to source.
Thanks for Your help and ideas,
Gerald