Part Number: TMS320F28379D
Other Parts Discussed in Thread: BOOSTXL-DRV8301, , DRV8301
I was trying to use the online Booster pack Compatibility Checker tool to check if I can use a BOOSTXL-DRV8301 booster pack with the TMS320F28379D launchpad as a quick prototype and the online tool lists that it is not compatible and there is a function mismatch on pin 29.
It lists the DRV8301 booster pack using this pin for the IC_FB signal (phase C current sensor feedback) and that the F28379 launchpad card uses this pin for CMPIN3N. However when I look at the F28379D quickstart guide it lists this pin as ADCINA2. Can someone confirm if the online compatibility checker tool is incorrect and the DRV8301 is actually compatible with the F28379D launchpad.