Other Parts Discussed in Thread: CONTROLSUITE, C2000WARE
Tool/software: Code Composer Studio
I was using ePWM to trigger ADC and i coded ADC's ISR such that the ADC's result is printed on the console every 30th conversion.I was also observing the ePWM's output on pin 80 of the launchpad
I observed a weird thing.Each time the result was printed on the console,Epwm's Output went to high state and stayed there for some time and then it began to function its own way((i.e.) it looked like a pure dc for some time and then it switched back to being a square wave) .Why did that happen? Am i wrong about the Epwm being independent of the C28x processor.(When i removed the printf statement the output was normal like it used to be - a square wave)
This was the code i used [highlighted parts are epwm configurations,the printf statement],
//###########################################################################
//
// FILE: adc_soc_epwm_cpu01.c
//
// TITLE: ADC triggering via epwm for F2837xS.
//
//! \addtogroup cpu01_example_list
//! <h1> ADC ePWM Triggering (adc_soc_epwm)</h1>
//!
//! This example sets up the ePWM to periodically trigger the ADC.
//!
//! After the program runs, the memory will contain:\n
//! - \b AdcaResults \b: A sequence of analog-to-digital conversion samples from
//! pin A0. The time between samples is determined based on the period
//! of the ePWM timer.
//
//###########################################################################
// $TI Release: F2837xS Support Library v210 $
// $Release Date: Tue Nov 1 15:35:23 CDT 2016 $
// $Copyright: Copyright (C) 2014-2016 Texas Instruments Incorporated -
// http://www.ti.com/ ALL RIGHTS RESERVED $
//###########################################################################
//
// Included Files
//
#include "F28x_Project.h"
#include "stdio.h"
#include "DCL.h"
const struct PIE_VECT_TABLE PieVectTableInit = {
PIE_RESERVED_ISR, // Reserved
PIE_RESERVED_ISR, // Reserved
PIE_RESERVED_ISR, // Reserved
PIE_RESERVED_ISR, // Reserved
PIE_RESERVED_ISR, // Reserved
PIE_RESERVED_ISR, // Reserved
PIE_RESERVED_ISR, // Reserved
PIE_RESERVED_ISR, // Reserved
PIE_RESERVED_ISR, // Reserved
PIE_RESERVED_ISR, // Reserved
PIE_RESERVED_ISR, // Reserved
PIE_RESERVED_ISR, // Reserved
PIE_RESERVED_ISR, // Reserved
TIMER1_ISR, // CPU Timer 1 Interrupt
TIMER2_ISR, // CPU Timer 2 Interrupt
DATALOG_ISR, // Datalogging Interrupt
RTOS_ISR, // RTOS Interrupt
EMU_ISR, // Emulation Interrupt
NMI_ISR, // Non-Maskable Interrupt
ILLEGAL_ISR, // Illegal Operation Trap
USER1_ISR, // User Defined Trap 1
USER2_ISR, // User Defined Trap 2
USER3_ISR, // User Defined Trap 3
USER4_ISR, // User Defined Trap 4
USER5_ISR, // User Defined Trap 5
USER6_ISR, // User Defined Trap 6
USER7_ISR, // User Defined Trap 7
USER8_ISR, // User Defined Trap 8
USER9_ISR, // User Defined Trap 9
USER10_ISR, // User Defined Trap 10
USER11_ISR, // User Defined Trap 11
USER12_ISR, // User Defined Trap 12
ADCA1_ISR, // 1.1 - ADCA Interrupt 1
ADCB1_ISR, // 1.2 - ADCB Interrupt 1
ADCC1_ISR, // 1.3 - ADCC Interrupt 1
XINT1_ISR, // 1.4 - XINT1 Interrupt
XINT2_ISR, // 1.5 - XINT2 Interrupt
ADCD1_ISR, // 1.6 - ADCD Interrupt 1
TIMER0_ISR, // 1.7 - Timer 0 Interrupt
WAKE_ISR, // 1.8 - Standby and Halt Wakeup Interrupt
EPWM1_TZ_ISR, // 2.1 - ePWM1 Trip Zone Interrupt
EPWM2_TZ_ISR, // 2.2 - ePWM2 Trip Zone Interrupt
EPWM3_TZ_ISR, // 2.3 - ePWM3 Trip Zone Interrupt
EPWM4_TZ_ISR, // 2.4 - ePWM4 Trip Zone Interrupt
EPWM5_TZ_ISR, // 2.5 - ePWM5 Trip Zone Interrupt
EPWM6_TZ_ISR, // 2.6 - ePWM6 Trip Zone Interrupt
EPWM7_TZ_ISR, // 2.7 - ePWM7 Trip Zone Interrupt
EPWM8_TZ_ISR, // 2.8 - ePWM8 Trip Zone Interrupt
EPWM1_ISR, // 3.1 - ePWM1 Interrupt
EPWM2_ISR, // 3.2 - ePWM2 Interrupt
EPWM3_ISR, // 3.3 - ePWM3 Interrupt
EPWM4_ISR, // 3.4 - ePWM4 Interrupt
EPWM5_ISR, // 3.5 - ePWM5 Interrupt
EPWM6_ISR, // 3.6 - ePWM6 Interrupt
EPWM7_ISR, // 3.7 - ePWM7 Interrupt
EPWM8_ISR, // 3.8 - ePWM8 Interrupt
ECAP1_ISR, // 4.1 - eCAP1 Interrupt
ECAP2_ISR, // 4.2 - eCAP2 Interrupt
ECAP3_ISR, // 4.3 - eCAP3 Interrupt
ECAP4_ISR, // 4.4 - eCAP4 Interrupt
ECAP5_ISR, // 4.5 - eCAP5 Interrupt
ECAP6_ISR, // 4.6 - eCAP6 Interrupt
PIE_RESERVED_ISR, // 4.7 - Reserved
PIE_RESERVED_ISR, // 4.8 - Reserved
EQEP1_ISR, // 5.1 - eQEP1 Interrupt
EQEP2_ISR, // 5.2 - eQEP2 Interrupt
EQEP3_ISR, // 5.3 - eQEP3 Interrupt
PIE_RESERVED_ISR, // 5.4 - Reserved
PIE_RESERVED_ISR, // 5.5 - Reserved
PIE_RESERVED_ISR, // 5.6 - Reserved
PIE_RESERVED_ISR, // 5.7 - Reserved
PIE_RESERVED_ISR, // 5.8 - Reserved
SPIA_RX_ISR, // 6.1 - SPIA Receive Interrupt
SPIA_TX_ISR, // 6.2 - SPIA Transmit Interrupt
SPIB_RX_ISR, // 6.3 - SPIB Receive Interrupt
SPIB_TX_ISR, // 6.4 - SPIB Transmit Interrupt
MCBSPA_RX_ISR, // 6.5 - McBSPA Receive Interrupt
MCBSPA_TX_ISR, // 6.6 - McBSPA Transmit Interrupt
MCBSPB_RX_ISR, // 6.7 - McBSPB Receive Interrupt
MCBSPB_TX_ISR, // 6.8 - McBSPB Transmit Interrupt
DMA_CH1_ISR, // 7.1 - DMA Channel 1 Interrupt
DMA_CH2_ISR, // 7.2 - DMA Channel 2 Interrupt
DMA_CH3_ISR, // 7.3 - DMA Channel 3 Interrupt
DMA_CH4_ISR, // 7.4 - DMA Channel 4 Interrupt
DMA_CH5_ISR, // 7.5 - DMA Channel 5 Interrupt
DMA_CH6_ISR, // 7.6 - DMA Channel 6 Interrupt
PIE_RESERVED_ISR, // 7.7 - Reserved
PIE_RESERVED_ISR, // 7.8 - Reserved
I2CA_ISR, // 8.1 - I2CA Interrupt 1
I2CA_FIFO_ISR, // 8.2 - I2CA Interrupt 2
I2CB_ISR, // 8.3 - I2CB Interrupt 1
I2CB_FIFO_ISR, // 8.4 - I2CB Interrupt 2
SCIC_RX_ISR, // 8.5 - SCIC Receive Interrupt
SCIC_TX_ISR, // 8.6 - SCIC Transmit Interrupt
SCID_RX_ISR, // 8.7 - SCID Receive Interrupt
SCID_TX_ISR, // 8.8 - SCID Transmit Interrupt
SCIA_RX_ISR, // 9.1 - SCIA Receive Interrupt
SCIA_TX_ISR, // 9.2 - SCIA Transmit Interrupt
SCIB_RX_ISR, // 9.3 - SCIB Receive Interrupt
SCIB_TX_ISR, // 9.4 - SCIB Transmit Interrupt
CANA0_ISR, // 9.5 - CANA Interrupt 0
CANA1_ISR, // 9.6 - CANA Interrupt 1
CANB0_ISR, // 9.7 - CANB Interrupt 0
CANB1_ISR, // 9.8 - CANB Interrupt 1
ADCA_EVT_ISR, // 10.1 - ADCA Event Interrupt
ADCA2_ISR, // 10.2 - ADCA Interrupt 2
ADCA3_ISR, // 10.3 - ADCA Interrupt 3
ADCA4_ISR, // 10.4 - ADCA Interrupt 4
ADCB_EVT_ISR, // 10.5 - ADCB Event Interrupt
ADCB2_ISR, // 10.6 - ADCB Interrupt 2
ADCB3_ISR, // 10.7 - ADCB Interrupt 3
ADCB4_ISR, // 10.8 - ADCB Interrupt 4
CLA1_1_ISR, // 11.1 - CLA1 Interrupt 1
CLA1_2_ISR, // 11.2 - CLA1 Interrupt 2
CLA1_3_ISR, // 11.3 - CLA1 Interrupt 3
CLA1_4_ISR, // 11.4 - CLA1 Interrupt 4
CLA1_5_ISR, // 11.5 - CLA1 Interrupt 5
CLA1_6_ISR, // 11.6 - CLA1 Interrupt 6
CLA1_7_ISR, // 11.7 - CLA1 Interrupt 7
CLA1_8_ISR, // 11.8 - CLA1 Interrupt 8
XINT3_ISR, // 12.1 - XINT3 Interrupt
XINT4_ISR, // 12.2 - XINT4 Interrupt
XINT5_ISR, // 12.3 - XINT5 Interrupt
PIE_RESERVED_ISR, // 12.4 - Reserved
PIE_RESERVED_ISR, // 12.5 - Reserved
VCU_ISR, // 12.6 - VCU Interrupt
FPU_OVERFLOW_ISR, // 12.7 - FPU Overflow Interrupt
FPU_UNDERFLOW_ISR, // 12.8 - FPU Underflow Interrupt
PIE_RESERVED_ISR, // 1.9 - Reserved
PIE_RESERVED_ISR, // 1.10 - Reserved
PIE_RESERVED_ISR, // 1.11 - Reserved
PIE_RESERVED_ISR, // 1.12 - Reserved
IPC0_ISR, // 1.13 - IPC Interrupt 0
IPC1_ISR, // 1.14 - IPC Interrupt 1
IPC2_ISR, // 1.15 - IPC Interrupt 2
IPC3_ISR, // 1.16 - IPC Interrupt 3
EPWM9_TZ_ISR, // 2.9 - ePWM9 Trip Zone Interrupt
EPWM10_TZ_ISR, // 2.10 - ePWM10 Trip Zone Interrupt
EPWM11_TZ_ISR, // 2.11 - ePWM11 Trip Zone Interrupt
EPWM12_TZ_ISR, // 2.12 - ePWM12 Trip Zone Interrupt
PIE_RESERVED_ISR, // 2.13 - Reserved
PIE_RESERVED_ISR, // 2.14 - Reserved
PIE_RESERVED_ISR, // 2.15 - Reserved
PIE_RESERVED_ISR, // 2.16 - Reserved
EPWM9_ISR, // 3.9 - ePWM9 Interrupt
EPWM10_ISR, // 3.10 - ePWM10 Interrupt
EPWM11_ISR, // 3.11 - ePWM11 Interrupt
EPWM12_ISR, // 3.12 - ePWM12 Interrupt
PIE_RESERVED_ISR, // 3.13 - Reserved
PIE_RESERVED_ISR, // 3.14 - Reserved
PIE_RESERVED_ISR, // 3.15 - Reserved
PIE_RESERVED_ISR, // 3.16 - Reserved
PIE_RESERVED_ISR, // 4.9 - Reserved
PIE_RESERVED_ISR, // 4.10 - Reserved
PIE_RESERVED_ISR, // 4.11 - Reserved
PIE_RESERVED_ISR, // 4.12 - Reserved
PIE_RESERVED_ISR, // 4.13 - Reserved
PIE_RESERVED_ISR, // 4.14 - Reserved
PIE_RESERVED_ISR, // 4.15 - Reserved
PIE_RESERVED_ISR, // 4.16 - Reserved
SD1_ISR, // 5.9 - SD1 Interrupt
SD2_ISR, // 5.10 - SD2 Interrupt
PIE_RESERVED_ISR, // 5.11 - Reserved
PIE_RESERVED_ISR, // 5.12 - Reserved
PIE_RESERVED_ISR, // 5.13 - Reserved
PIE_RESERVED_ISR, // 5.14 - Reserved
PIE_RESERVED_ISR, // 5.15 - Reserved
PIE_RESERVED_ISR, // 5.16 - Reserved
SPIC_RX_ISR, // 6.9 - *** Receive Interrupt
SPIC_TX_ISR, // 6.10 - *** Transmit Interrupt
PIE_RESERVED_ISR, // 6.11 - Reserved
PIE_RESERVED_ISR, // 6.12 - Reserved
PIE_RESERVED_ISR, // 6.13 - Reserved
PIE_RESERVED_ISR, // 6.14 - Reserved
PIE_RESERVED_ISR, // 6.15 - Reserved
PIE_RESERVED_ISR, // 6.16 - Reserved
PIE_RESERVED_ISR, // 7.9 - Reserved
PIE_RESERVED_ISR, // 7.10 - Reserved
PIE_RESERVED_ISR, // 7.11 - Reserved
PIE_RESERVED_ISR, // 7.12 - Reserved
PIE_RESERVED_ISR, // 7.13 - Reserved
PIE_RESERVED_ISR, // 7.14 - Reserved
PIE_RESERVED_ISR, // 7.15 - Reserved
PIE_RESERVED_ISR, // 7.16 - Reserved
PIE_RESERVED_ISR, // 8.9 - Reserved
PIE_RESERVED_ISR, // 8.10 - Reserved
PIE_RESERVED_ISR, // 8.11 - Reserved
PIE_RESERVED_ISR, // 8.12 - Reserved
PIE_RESERVED_ISR, // 8.13 - Reserved
PIE_RESERVED_ISR, // 8.14 - Reserved
#ifdef CPU1
UPPA_ISR, // 8.15 - uPPA Interrupt
PIE_RESERVED_ISR, // 8.16 - Reserved
#elif defined(CPU2)
PIE_RESERVED_ISR, // 8.15 - Reserved
PIE_RESERVED_ISR, // 8.16 - Reserved
#endif
PIE_RESERVED_ISR, // 9.9 - Reserved
PIE_RESERVED_ISR, // 9.10 - Reserved
PIE_RESERVED_ISR, // 9.11 - Reserved
PIE_RESERVED_ISR, // 9.12 - Reserved
PIE_RESERVED_ISR, // 9.13 - Reserved
PIE_RESERVED_ISR, // 9.14 - Reserved
#ifdef CPU1
USBA_ISR, // 9.15 - USBA Interrupt
#elif defined(CPU2)
PIE_RESERVED_ISR, // 9.15 - Reserved
#endif
PIE_RESERVED_ISR, // 9.16 - Reserved
ADCC_EVT_ISR, // 10.9 - ADCC Event Interrupt
ADCC2_ISR, // 10.10 - ADCC Interrupt 2
ADCC3_ISR, // 10.11 - ADCC Interrupt 3
ADCC4_ISR, // 10.12 - ADCC Interrupt 4
ADCD_EVT_ISR, // 10.13 - ADCD Event Interrupt
ADCD2_ISR, // 10.14 - ADCD Interrupt 2
ADCD3_ISR, // 10.15 - ADCD Interrupt 3
ADCD4_ISR, // 10.16 - ADCD Interrupt 4
PIE_RESERVED_ISR, // 11.9 - Reserved
PIE_RESERVED_ISR, // 11.10 - Reserved
PIE_RESERVED_ISR, // 11.11 - Reserved
PIE_RESERVED_ISR, // 11.12 - Reserved
PIE_RESERVED_ISR, // 11.13 - Reserved
PIE_RESERVED_ISR, // 11.14 - Reserved
PIE_RESERVED_ISR, // 11.15 - Reserved
PIE_RESERVED_ISR, // 11.16 - Reserved
EMIF_ERROR_ISR, // 12.9 - EMIF Error Interrupt
RAM_CORRECTABLE_ERROR_ISR, // 12.10 - RAM Correctable Error Interrupt
FLASH_CORRECTABLE_ERROR_ISR, // 12.11 - Flash Correctable Error Interrupt
RAM_ACCESS_VIOLATION_ISR, // 12.12 - RAM Access Violation Interrupt
SYS_PLL_SLIP_ISR, // 12.13 - System PLL Slip Interrupt
AUX_PLL_SLIP_ISR, // 12.14 - Auxiliary PLL Slip Interrupt
CLA_OVERFLOW_ISR, // 12.15 - CLA Overflow Interrupt
CLA_UNDERFLOW_ISR // 12.16 - CLA Underflow Interrupt
};
//
// InitPieVectTable - This function initializes the PIE vector table to a
// known state and must be executed after boot time.
//
void InitPieVectTable(void)
{
Uint16 i;
Uint32 *Source = (void *) &PieVectTableInit;
Uint32 *Dest = (void *) &PieVectTable;
//
// Do not write over first 3 32-bit locations (these locations are
// initialized by Boot ROM with boot variables)
//
Source = Source + 3;
Dest = Dest + 3;
EALLOW;
for(i = 0; i < 221; i++)
{
*Dest++ = *Source++;
}
EDIS;
//
// Enable the PIE Vector Table
//
PieCtrlRegs.PIECTRL.bit.ENPIE = 1;
}
//
// Function Prototypes
//
void ConfigureADC(void);
void ConfigureEPWM(void);
void SetupADCEpwm(Uint16 channel);
interrupt void adca1_isr(void);
//
// Defines
//
#define RESULTS_BUFFER_SIZE 256
//
// Globals
//
Uint16 AdcaResults[RESULTS_BUFFER_SIZE];
Uint16 resultsIndex;
volatile Uint16 bufferFull;
//PID pid1=PID_DEFAULTS;
/*struct hi
{
Uint16 ji:12
}bi;*/
int counter=0;
void main(void)
{//int counter=0;
//uk=DCL_runPIDc(&pid,)
//
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the F2837xS_SysCtrl.c file.
//
InitSysCtrl();
//
// Step 2. Initialize GPIO:
// This example function is found in the F2837xS_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
//
InitGpio(); // Skipped for this example
//
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
//
DINT;
InitGpio();
//
// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the F2837xS_PieCtrl.c file.
//
InitPieCtrl();
//
// Disable CPU interrupts and clear all CPU interrupt flags:
//
IER = 0x0000;
IFR = 0x0000;
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in F2837xS_DefaultIsr.c.
// This function is found in F2837xS_PieVect.c.
//
InitPieVectTable();
//
// Map ISR functions
//
EALLOW;
PieVectTable.ADCA1_INT = &adca1_isr; //function for ADCA interrupt 1
GpioCtrlRegs.GPAMUX1.bit.GPIO2=1;
EDIS;
//
// Configure the ADC and power it up
//
ConfigureADC();
//
// Configure the ePWM
//
ConfigureEPWM();
//
// Setup the ADC for ePWM triggered conversions on channel 0
//
SetupADCEpwm(0);
//
// Enable global Interrupts and higher priority real-time debug events:
//
IER |= M_INT1; //Enable group 1 interrupts
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
//
// Initialize results buffer
//
for(resultsIndex = 0; resultsIndex < RESULTS_BUFFER_SIZE; resultsIndex++)
{
AdcaResults[resultsIndex] = 0;
}
resultsIndex = 0;
bufferFull = 0;
//
// enable PIE interrupt
//
PieCtrlRegs.PIEIER1.bit.INTx1 = 1;
//
// sync ePWM
//
EALLOW;
CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 1;
PieCtrlRegs.PIECTRL.bit.ENPIE=1;
//
//take conversions indefinitely in loop
//
//EPwm2Regs.ETSEL.bit.SOCAEN = 1;
//EPwm2Regs.TBCTL.bit.CTRMODE = 0;
EDIS;
do
{
//
//start ePWM
//
//EPwm2Regs.ETSEL.bit.SOCAEN = 1; //enable SOCA
//EPwm2Regs.TBCTL.bit.CTRMODE = 0; //unfreeze, and enter up count mode
//
//wait while ePWM causes ADC conversions, which then cause interrupts,
//which fill the results buffer, eventually setting the bufferFull
//flag
//
//while(!bufferFull);
//bufferFull = 0; //clear the buffer full flag
//
//stop ePWM
//
//EPwm2Regs.ETSEL.bit.SOCAEN = 0; //disable SOCA
//EPwm2Regs.TBCTL.bit.CTRMODE = 3; //freeze counter
//
//at this point, AdcaResults[] contains a sequence of conversions
//from the selected channel
//
//
//software breakpoint, hit run again to get updated conversions
//
//asm(" ESTOP0");
}while(1);
}
//
// ConfigureADC - Write ADC configurations and power up the ADC for both
// ADC A and ADC B
//
void ConfigureADC(void)
{
EALLOW;
//
//write configurations
//
AdcaRegs.ADCCTL2.bit.PRESCALE = 6; //set ADCCLK divider to /4
AdcSetMode(ADC_ADCA, ADC_RESOLUTION_12BIT, ADC_SIGNALMODE_SINGLE);
//
//Set pulse positions to late
//
AdcaRegs.ADCCTL1.bit.INTPULSEPOS = 1;
//
//power up the ADC
//
AdcaRegs.ADCCTL1.bit.ADCPWDNZ = 1;
//
//delay for 1ms to allow ADC time to power up
//
DELAY_US(1000);
EDIS;
}
//
// ConfigureEPWM - Configure EPWM SOC and compare values
//
void ConfigureEPWM(void)
{
EALLOW;
// Assumes ePWM clock is already enabled
EPwm2Regs.ETSEL.bit.SOCAEN = 1; // Enable SOC on A group
EPwm2Regs.ETSEL.bit.SOCASEL = 4; // Select SOC on up-count
EPwm2Regs.ETPS.bit.SOCAPRD = 1; // Generate pulse on 1st event
EPwm2Regs.CMPA.bit.CMPA = 0x0800; // Set compare A value to 2048 counts
EPwm2Regs.TBPRD = 0x1000; // Set period to 4096 counts
EPwm2Regs.TBCTL.bit.CTRMODE = 0; // up counter
EPwm2Regs.AQCTLA.bit.CAU=2;
EPwm2Regs.AQCTLA.bit.PRD=1;
EDIS;
}
//
// SetupADCEpwm - Setup ADC EPWM acquisition window
//
void SetupADCEpwm(Uint16 channel)
{//EALLOW;
//GpioCtrlRegs.GPAMUX1.bit.GPIO13=0;
//GpioCtrlRegs.GPADIR.bit.GPIO13=1;
//EDIS;
//GpioDataRegs.GPASET.bit.GPIO13=1;
Uint16 acqps;
//
//determine minimum acquisition window (in SYSCLKS) based on resolution
//
if(ADC_RESOLUTION_12BIT == AdcaRegs.ADCCTL2.bit.RESOLUTION)
{
acqps = 63; //75ns
}
else //resolution is 16-bit
{
acqps = 63; //320ns
}
//
//Select the channels to convert and end of conversion flag
//
EALLOW;
AdcaRegs.ADCSOC0CTL.bit.CHSEL = channel; //SOC0 will convert pin A0
AdcaRegs.ADCSOC0CTL.bit.ACQPS = acqps; //sample window is 100 SYSCLK cycles
AdcaRegs.ADCSOC0CTL.bit.TRIGSEL = 7; //trigger on ePWM1 SOCA/C
AdcaRegs.ADCINTSEL1N2.bit.INT1SEL = 0; //end of SOC0 will set INT1 flag
AdcaRegs.ADCINTSEL1N2.bit.INT1E = 1; //enable INT1 flag
AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //make sure INT1 flag is cleared
// AdcaRegs.ADCPPB4CONFIG.bit.CONFIG=0;
// AdcaRegs.ADCPPB4CONFIG.bit.TWOSCOMPEN=0;
// AdcaRegs.ADCPPB4OFFCAL.bit.OFFCAL=0X64;
// AdcaRegs.ADCPPB4OFFREF=100;
EDIS;
}
//
// adca1_isr - Read ADC Buffer in ISR
//
interrupt void adca1_isr(void)
{
//AdcaResults[resultsIndex++] = AdcaResultRegs.ADCRESULT0;
//if(RESULTS_BUFFER_SIZE <= resultsIndex)
/* {
resultsIndex = 0;
bufferFull = 1;
}*/
counter++;
if(counter>30)
{printf("%d\n",AdcaResultRegs.ADCRESULT0);
counter=0;
}
//printf("%d\n",AdcaResultRegs.ADCPPB4RESULT.bit.PPBRESULT);
//resultsIndex = 0;
//bufferFull = 1;
/* if(AdcaResultRegs.ADCRESULT0==4095)
{
GpioDataRegs.GPACLEAR.bit.GPIO13=1;
}
}
*/
AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //clear INT1 flag
EALLOW;
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
EDIS;
}
//
// End of file
//