Other Parts Discussed in Thread: MOTORWARE, DRV8301, CONTROLSUITE, DRV8312
Tool/software: Code Composer Studio
Hello,
We have made a clone of DRV8301-HC-C2 kit for a competition but we are a little unsure of the code . Unfortunately we could not get the code to implement it on code composer studio.Please can anyone give me a code for :
1. An open loop circuit control of speed variation for 48V BLDC 3 phase motor ,which works on gate switching and power mosfets.
2. A closed loop circuit comprising of hall sensor for feedback for the same motor.
The battery capacity is 48V.
Please help us out ,it is urgent .
Also can anyone tell me if we can directly implement the code on a replica PCB using CCS7 but original Texas Instruments components placed on it.