Part Number: DRV8301-HC-C2-KIT
Tool/software: Code Composer Studio
Hello,
I have a replica of the kit DRV8301-HC-C2, made on a PCB using all the original components assembled.
I have been trying to find sample codes on motor control but have not yet found any on Control suite.
1. I need a code to implement an open loop for speed variation of a 48 v BLDC 3 phase motor .
2.Also a code to implement a closed circuit loop for the same motor.
Please forward the sample codes and the any good code urgently.
The battery capacity is 48V.