Part Number: TMS320F280049
My customer found CANB do not work in pin29/30 in his F280049 sample device. It can work if re-arrange the CANB to other pin such as pin 33/34 or pin 63/64.
After double check the pin signal arrangement in datasheet, it indeed describe that CANB is not available in pin29/30 for PMQ package, but should be available on pin29/30 for PMS package.
However customer sample device is XF280049MPMS, can we double confirm CANB should be available or not in pin29/30 for XF280049MPMS?
And customer actually need Q version for Automotive Application, however we cannot see PMQ device in the www.ti.com, when customer can order the Q version F280049?