Tool/software: TI C/C++ Compiler
I am trying to test the CAN Tx and Rx messages using the TMS320F 28335.
Where I am facing the problem of the code of the below and I am attaching the my main.c
Why always controller in the below mode
do
{
ECanaShadow.CANES.all = ECanaRegs.CANES.all;
} while(ECanaShadow.CANES.bit.CCE != 1 ); // Wait for CCE bit to be set..
I checked in the CANES register value is
/* ==============================================================================
Header files
=================================================================================*/
#include <stdlib.h>
#include "IQmathLib.h" /* Include header for IQmath library */
//#include "DSP2833x_Device.h" // DSP2833x Headerfile Include File
//#include "DSP2833x_Device.h" // DSP2833x Headerfile Include File
//#include "DSP2833x_Examples.h"
#include "DSP2833x_Device.h" // DSP2833x Headerfile Include File
#include "DSP2833x_Examples.h"
//#include "pmci.h"
//#include "parameter.h"
//#include "build.h"
//#include "DSP2833x_GlobalPrototypes.h" //for setting up SCI, SPI and XF
void mailbox_check(int32 T1, int32 T2, int32 T3);
void mailbox_read(int16 i);
// Global variable for this example
Uint32 ErrorCount;
Uint32 MessageReceivedCount;
Uint32 TestMbox1 = 0;
Uint32 TestMbox2 = 0;
Uint32 TestMbox3 = 0;
/*int main(void)
{
//InitECana();
hwi_can_init();
// CANtransmit();
//CAN_Receive();
return 0;
}
*/
void main(void)
{
Uint16 i,j;
// eCAN control registers require read/write access using 32-bits. Thus we
// will create a set of shadow registers for this example. These shadow
// registers will be used to make sure the access is 32-bits and not 16.
struct ECAN_REGS ECanaShadow;
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the DSP281x_SysCtrl.c file.
InitSysCtrl();
// Step 2. Initalize GPIO:
// This example function is found in the DSP281x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
//InitGpio(); // Skipped for this example
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
DINT;
// Initialize PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the DSP281x_PieCtrl.c file.
// InitPieCtrl(); // Skipped for this example
// Disable CPU interrupts and clear all CPU interrupt flags:
IER = 0x0000;
IFR = 0x0000;
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in DSP281x_DefaultIsr.c.
// This function is found in DSP281x_PieVect.c.
// InitPieVectTable(); // Skipped for this example
// Step 4. Initialize all the Device Peripherals:
// This function is found in DSP281x_InitPeripherals.c
// InitPeripherals(); // Not required for this example
// Step 5. User specific code
MessageReceivedCount = 0;
ErrorCount = 0;
EALLOW;
SysCtrlRegs.PCLKCR0.bit.ECANAENCLK= 1; // Enable system clk to eCAN-A
GpioCtrlRegs.GPAPUD.all = 0x0000; // Pullup's enabled GPIO0-GPIO31
InitECan(); // Initialize the eCAN module
// Mailboxs can be written to 16-bits or 32-bits at a time
// Write to the MSGID field of TRANSMIT mailboxes MBOX0 - 15
ECanaMboxes.MBOX0.MSGID.all = 0x9555AAA0;
ECanaMboxes.MBOX1.MSGID.all = 0x9555AAA1;
ECanaMboxes.MBOX2.MSGID.all = 0x9555AAA2;
ECanaMboxes.MBOX3.MSGID.all = 0x9555AAA3;
ECanaMboxes.MBOX4.MSGID.all = 0x9555AAA4;
ECanaMboxes.MBOX5.MSGID.all = 0x9555AAA5;
ECanaMboxes.MBOX6.MSGID.all = 0x9555AAA6;
ECanaMboxes.MBOX7.MSGID.all = 0x9555AAA7;
ECanaMboxes.MBOX8.MSGID.all = 0x9555AAA8;
ECanaMboxes.MBOX9.MSGID.all = 0x9555AAA9;
ECanaMboxes.MBOX10.MSGID.all = 0x9555AAAA;
ECanaMboxes.MBOX11.MSGID.all = 0x9555AAAB;
ECanaMboxes.MBOX12.MSGID.all = 0x9555AAAC;
ECanaMboxes.MBOX13.MSGID.all = 0x9555AAAD;
ECanaMboxes.MBOX14.MSGID.all = 0x9555AAAE;
ECanaMboxes.MBOX15.MSGID.all = 0x9555AAAF;
// Write to the MSGID field of RECEIVE mailboxes MBOX16 - 31
ECanaMboxes.MBOX16.MSGID.all = 0x9555BBB0;
ECanaMboxes.MBOX17.MSGID.all = 0x9555BBB1;
ECanaMboxes.MBOX18.MSGID.all = 0x9555BBB2;
ECanaMboxes.MBOX19.MSGID.all = 0x9555BBB3;
ECanaMboxes.MBOX20.MSGID.all = 0x9555BBB4;
ECanaMboxes.MBOX21.MSGID.all = 0x9555AAA5;
ECanaMboxes.MBOX22.MSGID.all = 0x9555AAA6;
ECanaMboxes.MBOX23.MSGID.all = 0x9555AAA7;
ECanaMboxes.MBOX24.MSGID.all = 0x9555AAA8;
ECanaMboxes.MBOX25.MSGID.all = 0x9555AAA9;
ECanaMboxes.MBOX26.MSGID.all = 0x9555AAAA;
ECanaMboxes.MBOX27.MSGID.all = 0x9555AAAB;
ECanaMboxes.MBOX28.MSGID.all = 0x9555AAAC;
ECanaMboxes.MBOX29.MSGID.all = 0x9555AAAD;
ECanaMboxes.MBOX30.MSGID.all = 0x9555AAAE;
ECanaMboxes.MBOX31.MSGID.all = 0x9555AAAF;
// Configure Mailboxes 0-15 as Tx, 16-31 as Rx
// Since this write is to the entire register (instead of a bit
// field) a shadow register is not required.
ECanaRegs.CANMD.all = 0xFFFF0000;
// Enable all Mailboxes */
// Since this write is to the entire register (instead of a bit
// field) a shadow register is not required.
ECanaRegs.CANME.all = 0xFFFFFFFF;
//ECanaRegs.CANME.all = 0x00010001;
// Specify that 8 bits will be sent
ECanaMboxes.MBOX0.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX1.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX2.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX3.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX4.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX5.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX6.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX7.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX8.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX9.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX10.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX11.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX12.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX13.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX14.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX15.MSGCTRL.bit.DLC = 8;
// Write to the mailbox RAM field of MBOX0 - 15
//ECanaMboxes.MBOX0.MDL.all = 0x9555AAA0;
//ECanaMboxes.MBOX0.MDH.all = 0x89ABCDEF;
ECanaMboxes.MBOX0.MDL.all = 0x11223344;
ECanaMboxes.MBOX0.MDH.all = 0x55667788;
ECanaMboxes.MBOX1.MDL.all = 0x9555AAA1;
ECanaMboxes.MBOX1.MDH.all = 0x89ABCDEF;
ECanaMboxes.MBOX2.MDL.all = 0x9555AAA2;
ECanaMboxes.MBOX2.MDH.all = 0x89ABCDEF;
ECanaMboxes.MBOX3.MDL.all = 0x9555AAA3;
ECanaMboxes.MBOX3.MDH.all = 0x89ABCDEF;
ECanaMboxes.MBOX4.MDL.all = 0x9555AAA4;
ECanaMboxes.MBOX4.MDH.all = 0x89ABCDEF;
ECanaMboxes.MBOX5.MDL.all = 0x9555AAA5;
ECanaMboxes.MBOX5.MDH.all = 0x89ABCDEF;
ECanaMboxes.MBOX6.MDL.all = 0x9555AAA6;
ECanaMboxes.MBOX6.MDH.all = 0x89ABCDEF;
ECanaMboxes.MBOX7.MDL.all = 0x9555AAA7;
ECanaMboxes.MBOX7.MDH.all = 0x89ABCDEF;
ECanaMboxes.MBOX8.MDL.all = 0x9555AAA8;
ECanaMboxes.MBOX8.MDH.all = 0x89ABCDEF;
ECanaMboxes.MBOX9.MDL.all = 0x9555AAA9;
ECanaMboxes.MBOX9.MDH.all = 0x89ABCDEF;
ECanaMboxes.MBOX10.MDL.all = 0x9555AAAA;
ECanaMboxes.MBOX10.MDH.all = 0x89ABCDEF;
ECanaMboxes.MBOX11.MDL.all = 0x9555AAAB;
ECanaMboxes.MBOX11.MDH.all = 0x89ABCDEF;
ECanaMboxes.MBOX12.MDL.all = 0x9555AAAC;
ECanaMboxes.MBOX12.MDH.all = 0x89ABCDEF;
ECanaMboxes.MBOX13.MDL.all = 0x9555AAAD;
ECanaMboxes.MBOX13.MDH.all = 0x89ABCDEF;
ECanaMboxes.MBOX14.MDL.all = 0x9555AAAE;
ECanaMboxes.MBOX14.MDH.all = 0x89ABCDEF;
ECanaMboxes.MBOX15.MDL.all = 0x9555AAAF;
ECanaMboxes.MBOX15.MDH.all = 0x89ABCDEF;
// Configure the eCAN for self test mode
// Enable the enhanced features of the eCAN.
ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
ECanaShadow.CANMC.bit.STM = 1; // Configure CAN for self-test mode
ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
/* Configure bit timing parameters for eCANA BaudRates */
ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
ECanaShadow.CANMC.bit.CCR = 1 ; // Set CCR = 1
ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
ECanaShadow.CANES.all = ECanaRegs.CANES.all;
do
{
ECanaShadow.CANES.all = ECanaRegs.CANES.all;
} while(ECanaShadow.CANES.bit.CCE != 1 ); // Wait for CCE bit to be set..
ECanaShadow.CANBTC.all = 0;
#if (CPU_FRQ_150MHZ) // CPU_FRQ_150MHz is defined in DSP2833x_Examples.h
/* The following block for all 150 MHz SYSCLKOUT (75 MHz CAN clock) - default. Bit rate = 1 Mbps
See Note at End of File */
ECanaShadow.CANBTC.bit.BRPREG = 9; // 4 for 1Mbps, 9 for 500Kbps, 19 for 250Kbps, 39 for 125Kbps, 49 for 100Kbps
ECanaShadow.CANBTC.bit.TSEG2REG = 2;
ECanaShadow.CANBTC.bit.TSEG1REG = 10;
#endif
#if (CPU_FRQ_100MHZ) // CPU_FRQ_100MHz is defined in DSP2833x_Examples.h
/* The following block is only for 100 MHz SYSCLKOUT (50 MHz CAN clock). Bit rate = 1 Mbps
See Note at End of File */
ECanaShadow.CANBTC.bit.BRPREG = 4; // 4 for 1Mbps, 9 for 500Kbps, 19 for 250Kbps, 39 for 125Kbps, 49 for 100Kbps
ECanaShadow.CANBTC.bit.TSEG2REG = 1;
ECanaShadow.CANBTC.bit.TSEG1REG = 6;
#endif
ECanaShadow.CANBTC.bit.SAM = 1;
ECanaRegs.CANBTC.all = ECanaShadow.CANBTC.all;
ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
ECanaShadow.CANMC.bit.CCR = 0 ; // Set CCR = 0
ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
ECanaShadow.CANES.all = ECanaRegs.CANES.all;
do
{
ECanaShadow.CANES.all = ECanaRegs.CANES.all;
} while(ECanaShadow.CANES.bit.CCE != 0 ); // Wait for CCE bit to be cleared..
//*********************************************************************
if (1){ // for the CAN A
//GpioCtrlRegs.GPADIR.bit.GPIO30 = 0; //0=input, 1=output
//GpioCtrlRegs.GPADIR.bit.GPIO31 = 1; //0=input, 1=output
//GpioCtrlRegs.GPAQSEL2.all = 0x0000; // GPIO16-GPIO31 Synch to SYSCLKOUT
//GpioCtrlRegs.GPAQSEL1.all = 0x05000000L; // No qualification for all group A GPIO 0-15
//GpioCtrlRegs.GPAQSEL2.all = 0x00000000L; // No qualification for all group A GPIO 16-31
GpioCtrlRegs.GPAPUD.bit.GPIO30 = 0; // Enable pullup on GPIO30
GpioCtrlRegs.GPAPUD.bit.GPIO31 = 0; // Enable pullup on GPIO31
GpioCtrlRegs.GPAQSEL2.bit.GPIO31 = 3; // Asynch input
GpioCtrlRegs.GPAMUX2.bit.GPIO30 = 1; //GPIO30: 0=GPIO, 1=CANRXA 2=rsvd 3=rsvd
GpioCtrlRegs.GPAMUX2.bit.GPIO31 = 1; //GPIO31: 0=GPIO, 1=CANTXA 2=rsvd 3=rsvd
// GpioCtrlRegs.GPACTRL.all = 0x00003200L; // QUALPRD = SYSCLKOUT for all group A GPIO
}
else{ // For the General Pupose IO
GpioCtrlRegs.GPAMUX2.bit.GPIO30 = 0; //GPIO30: 0=GPIO, 1=CANRXA 2=rsvd 3=rsvd
GpioCtrlRegs.GPAMUX2.bit.GPIO31 = 0; //GPIO31: 0=GPIO, 1=CANTXA 2=rsvd 3=rsvd
GpioCtrlRegs.GPADIR.bit.GPIO30 = 0; //0=input, 1=output
GpioCtrlRegs.GPADIR.bit.GPIO31 = 0; //0=input, 1=output
GpioCtrlRegs.GPAQSEL2.all = 0x0000; // GPIO16-GPIO31 Synch to SYSCLKOUT
};
//GpioDataRegs.GPADAT.bit.GPIO31 = 1;
//GpioDataRegs.GPASET.bit.GPIO31 =1;
// for (i=0;i<1000;i++){}//delay
// GpioDataRegs.GPADAT.bit.GPIO31 = 0;
//GpioDataRegs.GPACLEAR.bit.GPIO30 = 1;
//*******************************************************************8
EDIS;
// Begin transmitting
while(1)
{
//**************
// GpioDataRegs.GPADAT.bit.GPIO31 = 1;
//GpioDataRegs.GPASET.bit.GPIO31 =1;
// for (i=0;i<1000;i++){}//delay
// GpioDataRegs.GPADAT.bit.GPIO31 = 0;
//GpioDataRegs.GPACLEAR.bit.GPIO30 = 1;
//****************
ECanaRegs.CANTRS.all = 0x0000FFFC; // Set TRS for all transmit mailboxes
while(ECanaRegs.CANTA.all != 0x0000FFFC ) {} // Wait for all TAn bits to be set..
ECanaRegs.CANTA.all = 0x0000FFFC; // Clear all TAn
MessageReceivedCount++;
//Read from Receive mailboxes and begin checking for data */
for(j=16; j<31; j++) // Read & check 16 mailboxes
{
mailbox_read(j); // This func reads the indicated mailbox data
mailbox_check(TestMbox1,TestMbox2,TestMbox3); // Checks the received data
}
}
}
// This function reads out the contents of the indicated
// by the Mailbox number (MBXnbr).
void mailbox_read(int16 MBXnbr)
{
volatile struct MBOX *Mailbox;
Mailbox = &ECanaMboxes.MBOX0 + MBXnbr;
TestMbox1 = Mailbox->MDL.all; // = 0x9555AAAn (n is the MBX number)
TestMbox2 = Mailbox->MDH.all; // = 0x89ABCDEF (a constant)
TestMbox3 = Mailbox->MSGID.all;// = 0x9555BBBn (n is the MBX number)
} // MSGID of a rcv MBX is transmitted as the MDL data.
void mailbox_check(int32 T1, int32 T2, int32 T3)
{
if((T1 != T3) || ( T2 != 0x89ABCDEF))
{
ErrorCount++;
}
}
//===========================================================================
// No more.
//===========================================================================
/* Note:
As indicated in the 281x device errata (SPRZ193), double-reads/double writes should be
employed for accesses to the mailbox RAM & LAM/MOTO/MOTS areas. Note, however, that the
errata is applicable only if the mailbox RAM & LAM/MOTO/MOTS areas are accessed at the
same time. The header file example operates in self-test mode, with no possibility of
a contention. Hence, the workaround is not implemented. When eCAN is communicating with
another node in non self-test mode), the workaround must be incorporated.
*
Here I am attaching the screen shot of the CANES Register with value