Part Number: TMS320F28375S
Other Parts Discussed in Thread: CONTROLSUITE, C2000WARE
Team,
My customer is running into the following issue:
We finally have our first prototype boards with this processor. We’re using an external 16 MHz clock and desire to run the software from the internal PLL at 180 MHz. This required an IMULT of 11 and an FMULT of 0.25. Despite following the workarounds in the Errata SPRZ422 Ref F, we are still having a problem getting the PLL to lock consistently. We did not see this issue on the dev boards which were using a 10MHz oscillator and an IMULT of 18 and FMULT = 0. When we changed the FMULT from 0.25 to 0 on our board, the PLL seemed to lock right away every time (@ 176 MHz). Do you know if this issue is specifically related to using an FMULT other than 0? Do you think that should be added to the errata as a possible workaround?
We had a similar issue with an older processor (TMS320C6711) where the PLL would not lock and we had to drain the power supplies with every reset. Is the TMS320F28375 issue related to power supply or supply sequencing/timing?
They are going to run a few more experiments so any detailed or background information you can provide may help us understand the issue and come up with a reliable workaround.
Regards,
Aaron