This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TMS320F28377D: error #10099-D: program will not fit into available memory

Part Number: TMS320F28377D

Tool/software: TI C/C++ Compiler

Hello,

When I add one variable or one function, memory issue comes up. Could you please help me fix it?  What can I do for it to make it fit in?

Please see the following memory allocation.  Thanks!

MEMORY
{
PAGE 0 :
   /* BEGIN is used for the "boot to SARAM" bootloader mode   */

   BEGIN               : origin = 0x000000, length = 0x000002
   RAMM0               : origin = 0x000122, length = 0x0002DE
   RAMD0               : origin = 0x00B000, length = 0x000800
   RAMLS0              : origin = 0x008000, length = 0x000800
   RAMLS1              : origin = 0x008800, length = 0x000800
   RAMLS2              : origin = 0x009000, length = 0x000800
   RAMLS3              : origin = 0x009800, length = 0x000800
   RAMLS4              : origin = 0x00A000, length = 0x000800
   RESET               : origin = 0x3FFFC0, length = 0x000002

PAGE 1 :

   BOOT_RSVD       : origin = 0x000002, length = 0x000120     /* Part of M0, BOOT rom will use this for stack */
   RAMM1           : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */
   RAMD1           : origin = 0x00B800, length = 0x000800


   RAMLS5      : origin = 0x00A800, length = 0x000800

   RAMGS0      : origin = 0x00C000, length = 0x001000
   RAMGS1      : origin = 0x00D000, length = 0x001000
   RAMGS2      : origin = 0x00E000, length = 0x001000
   RAMGS3      : origin = 0x00F000, length = 0x001000
   RAMGS4      : origin = 0x010000, length = 0x001000
   RAMGS5      : origin = 0x011000, length = 0x001000
   RAMGS6      : origin = 0x012000, length = 0x001000
   RAMGS7      : origin = 0x013000, length = 0x001000
   RAMGS8      : origin = 0x014000, length = 0x001000
   RAMGS9      : origin = 0x015000, length = 0x001000
   RAMGS10     : origin = 0x016000, length = 0x001000
   RAMGS11     : origin = 0x017000, length = 0x001000
   RAMGS12     : origin = 0x018000, length = 0x001000
   RAMGS13     : origin = 0x019000, length = 0x001000
   RAMGS14     : origin = 0x01A000, length = 0x001000
   RAMGS15     : origin = 0x01B000, length = 0x001000
   
   CPU2TOCPU1RAM   : origin = 0x03F800, length = 0x000400
   CPU1TOCPU2RAM   : origin = 0x03FC00, length = 0x000400
}


SECTIONS
{
   codestart        : > BEGIN,     PAGE = 0
   ramfuncs         : >> RAMM0 | RAMLS2     PAGE = 0
   .text            : >> RAMM0 | RAMD0 |  RAMLS0 | RAMLS1 | RAMLS2 | RAMLS3| RAMLS4,   PAGE = 0
   .cinit           : > RAMM0,     PAGE = 0
   .pinit           : > RAMM0,     PAGE = 0
   .switch          : > RAMM0,     PAGE = 0
   .reset           : > RESET,     PAGE = 0, TYPE = DSECT /* not used, */

   .stack           : > RAMM1,     PAGE = 1
   .ebss            : > RAMLS5,    PAGE = 1
   .econst          : > RAMLS5,    PAGE = 1
   .esysmem         : > RAMLS5,    PAGE = 1
   Filter_RegsFile  : > RAMGS0,       PAGE = 1

   ramgs0           : > RAMGS0,    PAGE = 1
   ramgs1           : > RAMGS1,    PAGE = 1
   
   /* The following section definitions are required when using the IPC API Drivers */
    GROUP : > CPU1TOCPU2RAM, PAGE = 1
    {
        PUTBUFFER
        PUTWRITEIDX
        GETREADIDX
    }
    
    GROUP : > CPU2TOCPU1RAM, PAGE = 1
    {
        GETBUFFER :    TYPE = DSECT
        GETWRITEIDX :  TYPE = DSECT
        PUTREADIDX :   TYPE = DSECT
    }  
    
}

/*
//===========================================================================
// End of file.
//===========================================================================
*/