Part Number: TMS320F28377S
Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
Hi,
I configured ePWM2 using the example from C:\ti\c2000\C2000Ware_1_00_03_00\device_support\f2837xs\examples\cpu1\epwm_deadband and I have a problem. When I connected ePWM2A to the osciloscope I didn't see waveform. ePWM2A is always high on osciloscope.
#include "F28x_Project.h"
#define EPWM1_MAX_DB 0x03FF
#define EPWM2_MAX_DB 0x03FF
#define EPWM3_MAX_DB 0x03FF
#define EPWM1_MIN_DB 0
#define EPWM2_MIN_DB 0
#define EPWM3_MIN_DB 0
#define DB_UP 1
#define DB_DOWN 0
Uint32 EPwm2TimerIntCount;
Uint16 EPwm2_DB_Direction;
void InitEPwm2Example(void);
__interrupt void epwm2_isr(void);
void main(void)
{
InitSysCtrl();
CpuSysRegs.PCLKCR2.bit.EPWM2=1;
InitEPwm2Gpio();
DINT;
InitPieCtrl();
IER = 0x0000;
IFR = 0x0000;
InitPieVectTable();
EALLOW; // This is needed to write to EALLOW protected registers
PieVectTable.EPWM2_INT = &epwm2_isr;
EDIS;
EALLOW;
CpuSysRegs.PCLKCR0.bit.TBCLKSYNC =0;
EDIS;
InitEPwm2Example();
EALLOW;
CpuSysRegs.PCLKCR0.bit.TBCLKSYNC =1;
EDIS;
EPwm2TimerIntCount = 0;
IER |= M_INT3;
PieCtrlRegs.PIEIER3.bit.INTx2 = 1;
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
for(;;)
{
asm (" NOP");
}
}
// epwm2_isr - EPWM2 ISR
__interrupt void epwm2_isr(void)
{
if(EPwm2_DB_Direction == DB_UP)
{
if(EPwm2Regs.DBFED.bit.DBFED < EPWM2_MAX_DB)
{
EPwm2Regs.DBFED.bit.DBFED++;
EPwm2Regs.DBRED.bit.DBRED++;
}
else
{
EPwm2_DB_Direction = DB_DOWN;
EPwm2Regs.DBFED.bit.DBFED--;
EPwm2Regs.DBRED.bit.DBRED--;
}
}
else
{
if(EPwm2Regs.DBFED.bit.DBFED == EPWM2_MIN_DB)
{
EPwm2_DB_Direction = DB_UP;
EPwm2Regs.DBFED.bit.DBFED++;
EPwm2Regs.DBRED.bit.DBRED++;
}
else
{
EPwm2Regs.DBFED.bit.DBFED--;
EPwm2Regs.DBRED.bit.DBRED--;
}
}
EPwm2TimerIntCount++;
EPwm2Regs.ETCLR.bit.INT = 1;
PieCtrlRegs.PIEACK.all = PIEACK_GROUP3;
}
void InitEPwm2Example()
{
EPwm2Regs.TBPRD = 6000; // Set timer period
EPwm2Regs.TBPHS.bit.TBPHS = 0x0000; // Phase is 0
EPwm2Regs.TBCTR = 0x0000; // Clear counter
EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up
EPwm2Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Disable phase loading
EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV4; // Clock ratio to SYSCLKOUT
EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV4; // Slow just to observe on
// the scope
EPwm2Regs.CMPA.bit.CMPA = 3000;
EPwm2Regs.AQCTLA.bit.CAU = AQ_SET; // Set PWM2A on Zero
EPwm2Regs.AQCTLA.bit.CAD = AQ_CLEAR;
EPwm2Regs.AQCTLB.bit.CAU = AQ_CLEAR; // Set PWM2A on Zero
EPwm2Regs.AQCTLB.bit.CAD = AQ_SET;
EPwm2Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;
EPwm2Regs.DBCTL.bit.POLSEL = DB_ACTV_LOC;
EPwm2Regs.DBCTL.bit.IN_MODE = DBA_ALL;
EPwm2Regs.DBRED.bit.DBRED = EPWM2_MIN_DB;
EPwm2Regs.DBFED.bit.DBFED = EPWM2_MIN_DB;
EPwm2_DB_Direction = DB_UP;
EPwm2Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO; // Select INT on Zero event
EPwm2Regs.ETSEL.bit.INTEN = 1; // Enable INT
EPwm2Regs.ETPS.bit.INTPRD = ET_3RD; // Generate INT on 3rd event
}
Thank you in advance for your help
Best regards
Szymon