Part Number: TMS320F28335
Other Parts Discussed in Thread: CONTROLSUITE
Tool/software: Code Composer Studio
Recently I was transferring my program from CCS v5.1 to CCS v6.2. However, after I import my project into v6.2 and press compile, the problem below showed up.
I thought it is the problem about memory, so I modified the F28335_RAM_Ink.cmd as the following picture shows.
After this, it can compile successfully, but another problem showed up as below:
I have checked the program step by step. First, something weird happened when the program ran into "InitSysCtrl()".
It will stop at " asm(" ESTOP0") ". I'm a little bit confused of it.
and then I kept running the program, another trouble arouse in "InitAdc()" It happened in the command of DELAY_US(ADC_usDELAY) as below.
Hope someone could help me get through this, thanks.
By the way, this program is created in the version of v5.1, but I have created another new one in v6.1, and all those include file is from controlSuite v142.