Part Number: TMS320F28069M
Hi,
I have a BLDC solution where I need to maintain 10,000 RPM. The design is for a multi-volt appliance (110 / 220 VAC)
With Vdc Bus at 310VDC (220VAC input), 10K+ RPM is no issue.
With Vdc Bus at 155VDC (110VAC input), I can only achieve 7.5K RPM.
Wondering if there is an easy parameter change I can make to squeeze another 2500 RPM out of the design.?
Thanks
Stomp!