Part Number: TMS320F28033
Hi, my customer is using F28033 to build a DC/DC converter and in some situation the circuit will stop working, it's found that F28033 stopped working then.
We checked XRS, XCLKOUT, and VDDIO, and the waveform is as below.
XRS-blue, XCLKOUT-yellow, VDDIO-red.
It can be seen that XCLKOUT will have clock output for a short pulse and then high for about 3.5ms, repetitively.
After zoom in, the waveform is as below, the XCLKOUT output is always 60MHz=SYSCLK:
They are using an external crystal. And from the wavefrom we can know that F28033 does not reset during the period since XCLKOUT=SYSCLK, if reset, XCLKOUT=SYSCLK/4.
So they wonder
1. Can we determine that it's the input clock of the external crystal missing that caused XCLKOUT constant high? Is it possible that external crystal is still working but XCLKOUT output constant high(no clock pulse)?
2. Why F28033 does not reset when the clock is missing? How do we need to configure the registers that will let the MCU reset during missing clock input?