Other Parts Discussed in Thread: TMS320F28335, L293, CONTROLSUITE
Hi,
I'm developing on a F28335 DSP with the experimenter's kit, using CCS platinum 3.3. The setup has been working fine for weeks, but suddenly whenever I turn the unit on (plug it into the USB port), LD3 glows red, and I am unable to connect to the device. CCS usually crashes as a result.
The exact error message is ERROR 0x00000024/1137. It states that the device may be held in reset and suggests disconnecting and reconnecting all devices. I've done that a few times, even installed CCS on another machine. I've tried resetting the emulator, and Tying EMU 0/1 (pins 85 & 86) high through a resistor. Nothing seems to work.
Would someone be able to tell me how to get the chip back to the stage where I can connect to it and reprogram?
Thanks in advance,
Greg Stephenson