Tool/software: Code Composer Studio
Hi,
I need to synchronize the PWMs on different two DSPs (TMS320F28377D), sending the DSP1's EPWM1SYNCOUT signal to the DSP2's EXTSYNCIN1, please see below. I am not sure if this right or not. If it works, could you please help me with the following 2 questions? If it is wrong, could you please teach me how to do it? -Thanks!
1. How to configure INPUTXBAR5 to be EXTSYNCIN1 of DSP1?
2. How to configure EPWM1SYNCOUT of DSP1 to be the EXTSYNCIN1 of DSP2?
And the hardware connection is seen below. GPIO7 of DSP1 is connected with GPIO6 of DSP2, and GPIO6 of DSP1 is connected with GPIO7 of DSP2. Is this right?