Other Parts Discussed in Thread: TMDSCNCDH52C1, C2000WARE
Can you give a suggestion for a C2000 based microcontroller and Components needed for an application where the moste important interface is ethernet?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TMDSCNCDH52C1, C2000WARE
Can you give a suggestion for a C2000 based microcontroller and Components needed for an application where the moste important interface is ethernet?
Tom,
At the moment this is the only C2000 device with an integrated Ethernet Controller. This device is simpler that perhaps using a C2000 MCU like the F2806x and communicating over SPI with a TM4C129x running your Ethernet stack as the full application can run on a single chip.
Using the Concerto will allow you to run a c2000 application on the C28x core while the M3 is independently running an Ethernet stack. The C2000 can just periodically dump data across to the M3 core without worrying about managing the communication.
Thanks,
Mark