Part Number: LAUNCHXL-F28379D
#matlab #simulink #R2017b #externalmode #launchpad #F28379D
Hello LaunchPad-Fans,
right now I have a challenging problem and I wonder if someone can support me with this tricky issue.
I want to run my F28379D LaunchPad with Matlab/Simulink but I receive the error message below:
Error: Error occurred while executing External Mode MEX-file 'ext_comm':
Failed to connect to the target. A time-out occurred while waiting for the connection response from the target. Possible reasons for the time-out:
a) The target is not switched on.
b) The target is not connected to your host machine.
c) The application for the model is not running on the target. You might have clicked the Stop button. If the Run button is not dimmed, click it. Otherwise, click the Build button, which downloads and runs your application on the target.
Error:Unable to connect to the 'TI Delfino F2837xD' target for 'test_led'.
I have already set the required configurations in Simulink Hardware Configuration:
- Code Generation: Toolchain = Texas Instruments Code Composer Studio
- Hardware Board: F28379D
- Target hardware resources:
- Build options: Device Name = F28379D; don't boot from flash; CPU1; don't use custom linker
- External mode: Serial; COM10
Can you please help me with that issue so I can use the LaunchPad to scope signals in real time and tune parameters online.
Thank you for your valuable time and advice.
Johannes