Part Number: TMS320F2810
Hello,
I’m using the F2810PBKA and I have noticed this odd behavior of the ADC.
1st test: Vin = 0.1V continuous voltage without noise
ADC_result = 0.1V/3.0V*4095= 136bit
The 2810 result is correct = 136
2nd test : Vin = 0.11V continuous voltage with added a noise of 0.02Vpp (Signal Vmax=0.13V Vmin= 0.09V)
The 2810 result is always as it sees the Vmin= 0.09V/3.0V*4095= 122bit
Why does the ADC give always the minimum?
I’m using the ADC in simultaneuous sampling mode with the ADC (ADCLK) 25 MHz.
The same result happens if I work at ADCLK= 5 MHz.
Many Thanks for the support,
FAX