Part Number: LAUNCHXL-F28069M
Other Parts Discussed in Thread: MOTORWARE, DRV8301, BOOSTXL-DRV8301
Hello,
I am trying to implement code so that the 28069M launchpad is able to identify our custom VSI.
The goal:
To run a PMSM with a custom inverter and the 28069M launchpad
The system:
PMSM - Emrax 208, 300Vdc, 80kW motor, with RM44IE encoder
Custom VSI
LEM current sensors (no voltage sensors since we are using an encoder)
Launchpad - 28069M
Done so far:
We have been using the BOOSTXL-DRV8301 to get familiar with CCS and Instaspin. Have successfully completed most of the applicable motorware/instaspin labs (1, 2, 3, 5c, 12a - not getting accurate results because the DRV8301 cannot deliver the power needed which is understood).
We have designed a motherboard which fits on the 28069M and we have associated our necessary pins with those on the launchpad.
I have searched online for topics related to using the 28069M with a custom VSI and have failed to find anything. I have looked through the drv8301.c and .h files and I am at a loss. Any advice on where to start, and/or what to look for would be much appreciated.
Thank you,
Roberto