Part Number: TMS320F28335
Tool/software: Code Composer Studio
It seems as if, there is a limit on how many .c and .h on can add on TI's CCS 6 , 7.4 and perhaps the problem is all versions.
When adding a new .c or .h file via CCS method in a large project with many files, it seems as LINKER cannot tolerate any more file addition and gives the following error shown below
( NOTE: On reducing the number of files , even by 1 file the problem goes away and I get clean compile and successful Build, with checksum)
Add just 1 more more results in the following output from Code Composer Studio when linking: I never touched the make file or any other , except .c and .h
"C:/ti/ccsv7/tools/compiler/ti-cgt-c2000_16.9.6.LTS/bin/cl2000" -@"ccsLinker.opt" -o "steering.out"
makefile:371: recipe for target 'steering.out' failed
>> Unterminated quote in command file; aborting
Quote starts at "
gmake[1]: *** [steering.out] Error -1
makefile:367: recipe for target 'all' failed
gmake: *** [all] Error 2
I thought I has a bad character is one of my files, so I re-enterd all .c and .h all files and used CCS only to create and edit all the files.
TEXAS INSTRUMENT CCS experts please post ans show me how I can solve this problem.
I need to add more files, now my project is stuck!