This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LAUNCHXL-F28069M: on-chip Flash operation is different to RAM debug, what is the principle in cmd and system configuration between RAM Debug mode and Flash mode?

Part Number: LAUNCHXL-F28069M


Tool/software: Code Composer Studio

Hi,

I am working with LAUNCHXL-F28069M.

My code operate as I wish in RAM debug mode.

Then I modified cmd from "F2806x_CLA_C_lnk.cmd" as followed and wish to run in Flash mode but failed to operate as in RAM debug mode.

I've tested "Example_2806xFlash" and it works well with LAUNCHXL-F28069M.

What is the problem in my cmd file? or in my configuration?

My cmd file:(F2806x_Headers_nonBIOS.cmd is not modified)

-----------------------------------------------------------------------------------------------------------------------------------

--define=CLA_C=1
--define=_FLASH

_Cla1Prog_Start = _Cla1ProgRunStart;

MEMORY
{
PAGE 0 :   /* Program Memory */
           /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
   CLAPROGRAM  : origin = 0x009000, length = 0x001000      /* on-chip RAM block L3 */
   RAMM0       : origin = 0x000050, length = 0x0003B0     /* on-chip RAM block M0 */
   RAML5L8     : origin = 0x00C000, length = 0x008000
   OTP         : origin = 0x3D7800, length = 0x000400     /* on-chip OTP */

   FLASHH      : origin = 0x3D8000, length = 0x004000     /* on-chip FLASH */
   FLASHG      : origin = 0x3DC000, length = 0x004000     /* on-chip FLASH */
   FLASHF      : origin = 0x3E0000, length = 0x004000     /* on-chip FLASH */
   FLASHE      : origin = 0x3E4000, length = 0x004000     /* on-chip FLASH */
   FLASHD      : origin = 0x3E8000, length = 0x004000     /* on-chip FLASH */
   FLASHC      : origin = 0x3EC000, length = 0x004000     /* on-chip FLASH */
   FLASHA      : origin = 0x3F4000, length = 0x003F7E     /* on-chip FLASH */
   CSM_RSVD    : origin = 0x3F7F7E, length = 0x000076     /* Part of FLASHA.  Program with all 0x0000 when CSM is in use. */
   BEGIN       : origin = 0x3F7FF4, length = 0x000004     /* Part of FLASHA.  Used for "boot to Flash" bootloader mode. */
   CSM_PWL_P0  : origin = 0x3F7FF8, length = 0x000008     /* Part of FLASHA.  CSM password locations in FLASHA */

   FPUTABLES   : origin = 0x3FD860, length = 0x0006A0      /* FPU Tables in Boot ROM */
   IQTABLES    : origin = 0x3FDF00, length = 0x000B50     /* IQ Math Tables in Boot ROM */
   IQTABLES2   : origin = 0x3FEA50, length = 0x00008C     /* IQ Math Tables in Boot ROM */
   IQTABLES3   : origin = 0x3FEADC, length = 0x0000AA      /* IQ Math Tables in Boot ROM */

   ROM         : origin = 0x3FF3B0, length = 0x000C10     /* Boot ROM */
   RESET       : origin = 0x3FFFC0, length = 0x000002     /* part of boot ROM  */
   VECTORS     : origin = 0x3FFFC2, length = 0x00003E     /* part of boot ROM  */

PAGE 1 :   /* Data Memory */
           /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
           /* Registers remain on PAGE1                                                  */

   BOOT_RSVD   : origin = 0x000000, length = 0x000050     /* Part of M0, BOOT rom will use this for stack */
   RAMM1       : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */

   CLA1_MSGRAMLOW  : origin = 0x001480, length = 0x000080
   CLA1_MSGRAMHIGH : origin = 0x001500, length = 0x000080

   CLARAM0     : origin = 0x008800, length = 0x000400    /* on-chip RAM block L1 */
   CLARAM1     : origin = 0x008C00, length = 0x000400    /* on-chip RAM block L2 */
   CLARAM2     : origin = 0x008000, length = 0x000800    /* on-chip RAM block L0 */

   RAML4       : origin = 0x00A000, length = 0x002000     /* on-chip RAM block L4 */
   USB_RAM     : origin = 0x040000, length = 0x000800     /* USB RAM          */
   FLASHB      : origin = 0x3F0000, length = 0x004000     /* on-chip FLASH */
}

/* Allocate sections to memory blocks.
   Note:
         codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code
                   execution when booting to flash
         ramfuncs  user defined section to store functions that will be copied from Flash into RAM
*/


SECTIONS
{

   /* Allocate program areas: */
   codestart           : > BEGIN,      PAGE = 0
#if defined(RAM)
   .cinit              : > RAMM0,      PAGE = 0
   .pinit              : > RAMM0,      PAGE = 0
   .text               : > RAML5L8,    PAGE = 0
   ramfuncs            : > RAML5L8,    PAGE = 0
   .econst               : > RAML5L8,    PAGE = 0
   .switch             : > RAMM0,      PAGE = 0
    IQmath             : > RAML5L8,    PAGE = 0            /* Math Code */
   Cla1Prog            : {_Cla1ProgRunStart = .;} > CLAPROGRAM,
                                       PAGE = 0
   CLA1mathTables       : > CLARAM1,    PAGE = 1
#elif defined(_FLASH)
   .cinit              : > FLASHA,     PAGE = 0
   .pinit              : > FLASHA,     PAGE = 0
   .text               : > FLASHA,     PAGE = 0

   ramfuncs            : LOAD = FLASHD,
                         RUN = RAML5L8,
                         LOAD_START(_RamfuncsLoadStart),
                         RUN_START(_RamfuncsRunStart),
                         LOAD_SIZE(_RamfuncsLoadSize),
                         PAGE = 0
   /* Initalized sections to go in Flash */
   /* For SDFlash to program these, they must be allocated to page 0 */
   .econst             : > FLASHA,     PAGE = 0
   .switch             : > FLASHA,     PAGE = 0
   IQmath              : > FLASHA,     PAGE = 0            /* Math Code */

   Cla1Prog            : LOAD = FLASHD,
                         RUN = CLAPROGRAM,
                         LOAD_START(_Cla1ProgLoadStart),
                         LOAD_SIZE(_Cla1ProgLoadSize),
                         RUN_START(_Cla1ProgRunStart),
                         PAGE = 0

   CLA1mathTables       : LOAD = FLASHB,
                         RUN = CLARAM2,
                         LOAD_START(_CLA1mathTablesLoadStart),
                         LOAD_SIZE(_CLA1mathTablesLoadSize),
                         RUN_START(_CLA1mathTablesRunStart),
                         PAGE = 1
#else
#error Add either "RAM" or "_FLASH" to C2000 Linker -> Advanced Options -> Command File Preprocessing -> --define
#endif //RAM

   csmpasswds          : > CSM_PWL_P0, PAGE = 0
   csm_rsvd            : > CSM_RSVD,   PAGE = 0

   /* Allocate uninitalized data sections: */
   .stack              : > RAML4,      PAGE = 1
   .ebss               : > RAML4,      PAGE = 1
   .esysmem            : > RAML4,      PAGE = 1

   /* Allocate IQ math areas: */
   IQmathTables        : > IQTABLES,   PAGE = 0, TYPE = NOLOAD

   /* Allocate FPU math areas: */
   FPUmathTables       : > FPUTABLES,  PAGE = 0, TYPE = NOLOAD

   Cla1ToCpuMsgRAM  : > CLA1_MSGRAMLOW,   PAGE = 1
   CpuToCla1MsgRAM  : > CLA1_MSGRAMHIGH,  PAGE = 1
   Cla1DataRam0        : > CLARAM0,          PAGE = 1
   Cla1DataRam1        : > CLARAM1,          PAGE = 1
   Cla1DataRam2        : > CLARAM2,          PAGE = 1

   /* Allocate CLA 'C' Areas */
#ifdef CLA_C
   /* CLA C compiler sections */
   //
   // Must be allocated to memory the CLA has write access to
   //
   .scratchpad      : > CLARAM1,       PAGE = 1
   .bss_cla            : > CLARAM2,       PAGE = 1
   .const_cla        : > CLARAM2,       PAGE = 1
#endif //CLA_C


  /* Uncomment the section below if calling the IQNexp() or IQexp()
      functions from the IQMath.lib library in order to utilize the
      relevant IQ Math table in Boot ROM (This saves space and Boot ROM
      is 1 wait-state). If this section is not uncommented, IQmathTables2
      will be loaded into other memory (SARAM, Flash, etc.) and will take
      up space, but 0 wait-state is possible.
   */
   /*
   IQmathTables2    : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
   {

              IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)

   }
   */
    /* Uncomment the section below if calling the IQNasin() or IQasin()
       functions from the IQMath.lib library in order to utilize the
       relevant IQ Math table in Boot ROM (This saves space and Boot ROM
       is 1 wait-state). If this section is not uncommented, IQmathTables2
       will be loaded into other memory (SARAM, Flash, etc.) and will take
       up space, but 0 wait-state is possible.
    */
    /*
    IQmathTables3    : > IQTABLES3, PAGE = 0, TYPE = NOLOAD
    {

               IQmath.lib<IQNasinTable.obj> (IQmathTablesRam)

    }
    */

   /* .reset is a standard section used by the compiler.  It contains the */
   /* the address of the start of _c_int00 for C Code.   /*
   /* When using the boot ROM this section and the CPU vector */
   /* table is not needed.  Thus the default type is set here to  */
   /* DSECT  */
   .reset              : > RESET,      PAGE = 0, TYPE = DSECT
   vectors             : > VECTORS,    PAGE = 0, TYPE = DSECT

}

-----------------------------------------------------------------------------------------------------------------------------------------

Main.c file:


-----------------------------------------------------------------------------------------------------------------------------------------

#include "DSP28x_Project.h"     // Device Headerfile and Examples Include File
#include "Init.h"

// These are defined by the linker
#ifdef FLASH
    extern Uint16 RamfuncsLoadStart;
    extern Uint16 RamfuncsRunStart;
    extern Uint16 RamfuncsLoadSize;
#endif

void main(void)
{
    DINT;

    InitSysCtrl();

#ifdef FLASH
    memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (Uint32)&RamfuncsLoadSize);
    InitFlash();
#endif

    InitGpio();

    DINT;

    InitPieCtrl();
    IER = 0x0000;
    IFR = 0x0000;
    InitPieVectTable();

    InitCpuTimers();
    InitCLA();
    InitADC();
    InitEPwm();
    InitECAN();
    InitSCI();
    InitSPI();
    InitI2C();

    EINT;   // Enable Global interrupt INTM
    ERTM;   // Enable Global realtime interrupt DBGM

//    Cla1ForceTask8andWait();

    while(1){

    }

}


-----------------------------------------------------------------------------------------------------------------------------------------

Thanks,

Chen

LAUNCHXL-F28069M

  • Hello, Chen
    What is the problem? You can't build the project? Or it doesn't load to memory? Or it fails while running?
  • Hi Disona,

    Project can be built and load to flash.
    However, it doesn't work properly. For example, in RAM mode pwm generated but in Flash mode no signal is generated.
  • Hm. Do you load your project with JTAG? Can you set a breakpoint after "InitEPwm()" and ensure that EPwm Registers are inited properly?
    Do you have "FLASH" deifinition in your "main.c"? I can see you have "--define=_FLASH" in your "cmd" but no "#define FLASH" in your main.
  • Hi Disona,

    Thanks for your reply.
    On board XDS100V2 is used to load the project. #define FLASH is done in "init.h".
    When I load the project in CCS and debug, it operates correct. However, after power off and power on again, it doesnt work.

    Chen
  • Maybe you should call "memcpy()" three times? Because i can see, that you have "Cla1Prog" and "CLA1mathTables" section, that must be copied to RAM from flash, but you call "memcpy()" only for "ramfuncs" section.

    Or is it done in "InitCLA()"?

  • Em, memcpy() of Cla1Prog is done in InitCLA().

    I've checked the map file. Something is different between my project and Example_2806xFlash as followed.
    In Example, its Example_28069Flash.c file(Example_28069Flash.obj ) is a part of input section of ramfuncs.
    But in my project, main.c file(main.obj) doesn't included in ramfuncs.
    What's the reason?

    In Example:
    -----------------------------------------------------------------------------------------
    output attributes/
    section page origin length input sections
    -------- ---- ---------- ---------- ----------------
    ramfuncs 0 003e8000 00000063 RUN ADDR = 00008000
    003e8000 00000044 Example_28069Flash.obj (ramfuncs:retain)
    003e8044 0000001b F2806x_SysCtrl.obj (ramfuncs)
    003e805f 00000004 F2806x_usDelay.obj (ramfuncs)
    ------------------------------------------------------------------------------------------

    In my project:
    ------------------------------------------------------------------------------------------
    ramfuncs 0 003e80c0 0000001f RUN ADDR = 0000c000
    003e80c0 0000001b F2806x_SysCtrl.obj (ramfuncs)
    003e80db 00000004 F2806x_usDelay.obj (ramfuncs)
    ------------------------------------------------------------------------------------------
  • You see that because of interrupts placed into ramfuncs section in the example:
    #pragma CODE_SECTION(epwm1_timer_isr, "ramfuncs");
    #pragma CODE_SECTION(epwm2_timer_isr, "ramfuncs");

    If you will have some functions in your "main.c", that must be copied in RAM, you will see "retain" in your map-file too. It's ok.
    The problem is somwhere else.
  • Hi Chen,

    Can you give an update on this - are you still seeing issues where the PWM signal is not generated in Flash configuration?
    I've reviewed your linker command file and it looks fine. I see that you're using RAML3 for CLA program code which is correct.

    An example that may be helpful to look at and compare with your project:
    Example_2806xClaAdcFirFlash

    Regards,
    Elizabeth
  • Hi Elizabeth,

    The problem is sure located in linker command file.

    I recode my cmd file and it works correct.

    new cmd code is :

    ________________________________________________________________________

    _Cla1Prog_Start=_Cla1ProgRunStart;

    MEMORY
    {
    PAGE 0: /* Program Memory */
    CLAPROGRAM : origin = 0x009000, length = 0x001000 /* on-chip RAM block L3 */
    /* RAML0 : origin = 0x008000, length = 0x000800 */ /* on-chip RAM block L0 */
    /* RAML1 : origin = 0x008800, length = 0x000400 */ /* on-chip RAM block L1 */
    /* RAMM0 : origin = 0x000050, length = 0x0003B0 */ /* on-chip RAM block M0 */
    /* RAML5L8 : origin = 0x00C000, length = 0x008000 */
    RAML8 : origin = 0x012000, length = 0x002000 /* on-chip RAM block L8 */
    OTP : origin = 0x3D7800, length = 0x000400 /* on-chip OTP */

    FLASHH : origin = 0x3D8000, length = 0x004000 /* on-chip FLASH */
    FLASHG : origin = 0x3DC000, length = 0x004000 /* on-chip FLASH */
    FLASHF : origin = 0x3E0000, length = 0x004000 /* on-chip FLASH */
    FLASHE : origin = 0x3E4000, length = 0x004000 /* on-chip FLASH */
    FLASHD : origin = 0x3E8000, length = 0x004000 /* on-chip FLASH */
    FLASHC : origin = 0x3EC000, length = 0x004000 /* on-chip FLASH */
    FLASHA : origin = 0x3F4000, length = 0x003F80 /* on-chip FLASH */

    CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */
    BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */
    CSM_PWL_P0 : origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */

    FPUTABLES : origin = 0x3FD860, length = 0x0006A0 /* FPU Tables in Boot ROM */
    IQTABLES : origin = 0x3FDF00, length = 0x000B50 /* IQ Math Tables in Boot ROM */
    IQTABLES2 : origin = 0x3FEA50, length = 0x00008C /* IQ Math Tables in Boot ROM */
    IQTABLES3 : origin = 0x3FEADC, length = 0x0000AA /* IQ Math Tables in Boot ROM */

    ROM : origin = 0x3FF3B0, length = 0x000C10 /* Boot ROM */
    RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */
    VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */

    PAGE 1: /* Data Memory */
    BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */
    RAMM0 : origin = 0x000050, length = 0x0003B0 /* on-chip RAM block M0 */
    RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
    /* RAML2 : origin = 0x008C00, length = 0x000400 */ /* on-chip RAM block L2 */
    RAML3 : origin = 0x009000, length = 0x001000 /* on-chip RAM block L3 */
    RAML4 : origin = 0x00A000, length = 0x002000 /* on-chip RAM block L4 */
    RAML5 : origin = 0x00C000, length = 0x002000 /* on-chip RAM block L5 */
    RAML6 : origin = 0x00E000, length = 0x002000 /* on-chip RAM block L6 */
    RAML7 : origin = 0x010000, length = 0x002000 /* on-chip RAM block L7 */

    CLA1_MSGRAMLOW : origin = 0x001480, length = 0x000080
    CLA1_MSGRAMHIGH : origin = 0x001500, length = 0x000080

    CLARAM0 : origin = 0x008800, length = 0x000400 /* on-chip RAM block L1 */
    CLARAM1 : origin = 0x008C00, length = 0x000400 /* on-chip RAM block L2 */
    CLARAM2 : origin = 0x008000, length = 0x000800 /* on-chip RAM block L0 */

    USB_RAM : origin = 0x040000, length = 0x000800 /* USB RAM */
    FLASHB : origin = 0x3F0000, length = 0x004000 /* on-chip FLASH */
    }

    SECTIONS
    {
    /* Allocate program areas: */
    .cinit : > FLASHA, PAGE = 0
    .pinit : > FLASHA, PAGE = 0
    .text : > FLASHA, PAGE = 0

    codestart : > BEGIN, PAGE = 0
    ramfuncs : LOAD = FLASHD,
    RUN = RAML8,
    LOAD_START(_RamfuncsLoadStart),
    LOAD_END(_RamfuncsLoadEnd),
    RUN_START(_RamfuncsRunStart),
    LOAD_SIZE(_RamfuncsLoadSize),
    PAGE = 0

    /* Allocate CLA areas */
    Cla1Prog : LOAD = FLASHE,
    RUN = CLAPROGRAM,
    LOAD_START(_Cla1ProgLoadStart),
    LOAD_SIZE(_Cla1ProgLoadSize),
    RUN_START(_Cla1ProgRunStart),
    PAGE = 0

    CLA1mathTables : LOAD = FLASHB,
    RUN = CLARAM2,
    LOAD_START(_CLA1mathTablesLoadStart),
    LOAD_SIZE(_CLA1mathTablesLoadSize),
    RUN_START(_CLA1mathTablesRunStart),
    PAGE = 1

    Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW, PAGE = 1
    CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH, PAGE = 1
    Cla1DataRam0 : > CLARAM0, PAGE = 1
    Cla1DataRam1 : > CLARAM1, PAGE = 1
    Cla1DataRam2 : > CLARAM2, PAGE = 1

    /* Allocate CLA ‘C’ Areas */
    .scratchpad : > CLARAM1, PAGE = 1
    .bss_cla : > CLARAM2, PAGE = 1
    .const_cla : > CLARAM2, PAGE = 1

    /* Initialized sections to go in Flash */
    /* For SDFlash to program these, they must be allocated to page 0 */
    .econst : > FLASHA, PAGE = 0
    .switch : > FLASHA, PAGE = 0

    csmpasswds : > CSM_PWL_P0, PAGE = 0
    csm_rsvd : > CSM_RSVD, PAGE = 0

    /* Allocate uninitialized data sections */
    .stack : > RAMM0, PAGE = 1
    .ebss : > RAML4, PAGE = 1
    .esysmem : > RAML5, PAGE = 1

    /* Allocate IQ math areas */
    IQmath : > FLASHA, PAGE = 0
    IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD

    /* Allocate FPU math areas */
    FPUmathTables : > FPUTABLES, PAGE = 0, TYPE = NOLOAD

    /* .reset is a standard section used by the compiler. */
    /* It contains the address of the start of _c_int00 for C code. */
    /* When using the boot ROM, this section and the CPU vector table is not needed. */
    /* Thus the default type is set here to DSECT. */
    .reset : > RESET, PAGE = 0, TYPE = DSECT
    vectors : > VECTORS, PAGE = 0, TYPE = DSECT

    }

    _____________________________________________________________________