Part Number: C2000-GANG
Other Parts Discussed in Thread: F28M36P63C2
Hi,
Please tell me about Verify function of GUI.
We are using C2000-GANG for writing F28M36P63C2.
I want to execute only Verify on both the ARM core and the C28 core area for the device programmed with C2000-GANG.
When selecting the device of the group of "F28M3x Concerto" as the MCU Type, by checking the item of "Program all cores enable (GO button)",
for the memory of the two cores of ARM (Coretex-M3) core and C28 core , "GO (F9)" button execution "Erase -> Blank Check -> Program -> Verify"
will be executed continuously.
In the case of the "verify" button, since Verify is executed only for the selected core, it is necessary to select and execute the ARM core and C28 core.
Is there a setting to run Verify continuously for the ARM core and the C28 core Flash memory with one click like the "Go" button?
Thank you
Best Regards,
Koichi