Part Number: LAUNCHXL-F28069M
Other Parts Discussed in Thread: CONTROLSUITE, C2000WARE
Tool/software: Code Composer Studio
Hello! I've downloaded controlSUITE for the example code to get started with the C2000, but I think i'm missing something!
I tried downloading the timed_led_blink and a few others, but I seem to missing the header files. Then, when I add those header files, they seem to require more files. I always seem to end up getting lost in the amount of files I have to add, and then I got a boatload of error which I give up on.
Heres what Im doing:
1. Copying "timed_led_blink" onto my computer
2. Importing that into CCS
3. Clicking Run
3.i. The first error I get, is the XDAIS error, which I learned how to fix
3.ii. Then I need to include "DSP28x_Project.h"
This is where I believe theres an easier solution. I pulled "DSP28x_Project.h" from another example folder, but that needs even more files.
Is there an easier way to do this? Under 'Supporting Libraries', I notice theres 'Header Files for F2806x, but thats an expandable list which goes into more lists, Im not sure what to do.
What should I do?
I attached a picture of controlSUITE with what im seeing and some of my questions:
Also, Is there any standalone projects I can import and begin to program this guy?
If there's any more info you need, ill be eager to reply!