This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377S: EPWM: EPWMSYNCOUTEN register

Part Number: TMS320F28377S


Is EPWMSYNCOUTEN register actually available on the 28377S?

Looks like it was added in revision E of the TRM (SPRUHX5), together with EPWMSYNCINSEL.

According to this thread, EPWMSYNCINSEL does not actually exist (at least on 28377D):

Is EPWMSYNCOUTEN a typo as well?

Thank you!

-Pavel

  • Yes You are correct. Unfortunately that is a mistake in the documentation generation. Neither EPWMSYNCOUTEN or EPWMSYNCINSEL are available in this devices. The registers will be removed in the next rev of the TRM.

    Thank you for bringing this to our attention.