Part Number: TMS320F28377D
Hi all,
I have written the code for generating three phase shifted PWM signals using EPWM1, EPWM2 and EPWM3 channels as shown in the picture. However, after running the code I can not see any signals coming out of the channels.
Could you please help me finding what wrong am I doing with the code?
Best regards,
Haque
main.c
#include "F28x_Project.h"
//#include "adc_new.h"
#include "pwm.h"
int main (void)
{
InitSysCtrl();
pwm_init();
// ADC_init();
while (1) {
asm ("NOP");
}
return (1);
}
pwm.c
#include "pwm.h"
//#include "modulator_instance.h"
//#include "adc_new.h"
//#include "PLL.h"
//#include "measurement.h"
//unsigned int comp;
float duty_p1;
float duty_p2;
float duty_p3;
void pwm_init()
{
//enable PWM modules+ for three converter
CpuSysRegs.PCLKCR2.bit.EPWM1 = 1;
CpuSysRegs.PCLKCR2.bit.EPWM2 = 1;
CpuSysRegs.PCLKCR2.bit.EPWM3 = 1;
//Configure output pins for three converter
InitEPwm1Gpio();
InitEPwm2Gpio();
InitEPwm3Gpio();
//configure interrupt
DINT;
InitPieCtrl();
// Disable CPU interrupts and clear all CPU interrupt flags:
IER = 0x0000;
IFR = 0x0000;
InitPieVectTable();
EALLOW;
PieVectTable.EPWM1_INT = &pwm_interrupt;
EDIS; // This is needed to disable write to EALLOW protected registers
//setup PWM channels...
EALLOW;
CpuSysRegs.PCLKCR0.bit.TBCLKSYNC =0;
EDIS;
configure_pwm1();
configure_pwm2();
configure_pwm3();
EALLOW;
CpuSysRegs.PCLKCR0.bit.TBCLKSYNC =1;
EDIS;
// enable PIE interrupts
IER |= M_INT3;
PieCtrlRegs.PIEIER3.bit.INTx1 = 1;
// configure a pin for interrupt usage...
EALLOW;
GpioCtrlRegs.GPADIR.bit.GPIO13 = 1;
EDIS;
// enable interrupts, openloop will start...
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
}
void configure_pwm1()
{
EPwm1Regs.TBPRD = 1250; // Set timer period
EPwm1Regs.TBPHS.bit.TBPHS = 0x0000; // Phase is 0
EPwm1Regs.TBCTR = 0x0000; // Clear counter
// Setup TBCLK
EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up
EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Disable phase loading
EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // Clock ratio to SYSCLKOUT
EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV2;
EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; // Load registers every ZERO
EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
}
void configure_pwm2()
{
EPwm2Regs.TBPRD = 1250; // Set timer period
EPwm2Regs.TBPHS.bit.TBPHS = 0x009C; // Phase is 45 degree (TBPHS 156)
EPwm2Regs.TBCTR = 0x0000; // Clear counter
// Setup TBCLK
EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up
EPwm2Regs.TBCTL.bit.PHSEN = TB_ENABLE; // Enable phase loading
EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // Clock ratio to SYSCLKOUT
EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV2;
EPwm2Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; // Load registers every ZERO
EPwm2Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm2Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
EPwm2Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
}
void configure_pwm3()
{
EPwm3Regs.TBPRD = 1250; // Set timer period
EPwm3Regs.TBPHS.bit.TBPHS = 0x0138; // Phase is 90 degree (TBPHS 312)
EPwm3Regs.TBCTR = 0x0000; // Clear counter
// Setup TBCLK
EPwm3Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up
EPwm3Regs.TBCTL.bit.PHSEN = TB_ENABLE; // Enable phase loading
EPwm3Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // Clock ratio to SYSCLKOUT
EPwm3Regs.TBCTL.bit.CLKDIV = TB_DIV2;
EPwm3Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; // Load registers every ZERO
EPwm3Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm3Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
EPwm3Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
}
__interrupt void pwm_interrupt (void)
{
GpioDataRegs.GPASET.bit.GPIO13 = 1;
// doall measurement()
// pll tick
// series volt reg tick
// shunt reg tick
// dc bus reg tick
//set duty cycles for series converter
duty_p1 = (float)PWM_PERIOD / 2;
EPwm1Regs.CMPA.bit.CMPA = (int) duty_p1;
EPwm1Regs.CMPB.bit.CMPB = (int) duty_p1;
// Set actions
EPwm1Regs.AQCTLA.bit.CAU = AQ_SET; // Set PWM1A on Zero
EPwm1Regs.AQCTLA.bit.CAD = AQ_CLEAR;
EPwm1Regs.AQCTLB.bit.CAU = AQ_CLEAR; // Set PWM1B on Zero
EPwm1Regs.AQCTLB.bit.CAD = AQ_SET;
duty_p2 = (float)PWM_PERIOD / 2;
EPwm2Regs.CMPA.bit.CMPA = (int) duty_p2;
EPwm2Regs.CMPB.bit.CMPB = (int) duty_p2;
// Set actions
EPwm2Regs.AQCTLA.bit.CAU = AQ_SET; // Set PWM1A on Zero
EPwm2Regs.AQCTLA.bit.CAD = AQ_CLEAR;
EPwm2Regs.AQCTLB.bit.CAU = AQ_CLEAR; // Set PWM1A on Zero
EPwm2Regs.AQCTLB.bit.CAD = AQ_SET;
duty_p3 = (float)PWM_PERIOD / 2;
EPwm3Regs.CMPA.bit.CMPA = (int) duty_p3;
EPwm3Regs.CMPB.bit.CMPB = (int) duty_p3;
// Set actions
EPwm3Regs.AQCTLA.bit.CAU = AQ_SET; // Set PWM1A on Zero
EPwm3Regs.AQCTLA.bit.CAD = AQ_CLEAR;
EPwm3Regs.AQCTLB.bit.CAU = AQ_CLEAR; // Set PWM1B on Zero
EPwm3Regs.AQCTLB.bit.CAD = AQ_SET;
EPwm1Regs.ETCLR.bit.INT = 1;
PieCtrlRegs.PIEACK.all = PIEACK_GROUP3;
GpioDataRegs.GPACLEAR.bit.GPIO13 = 1;
}
pwm.h
#ifndef PWM_H_
#define PWM_H_
#include "F28x_Project.h"
//#include "sine_modulator.h"
#define PWM_PERIOD 1250
extern float duty_p1;
extern float duty_p2;
extern float duty_p3;
void pwm_init();
// PWM 1~3 for three converters
void configure_pwm1();
void configure_pwm2();
void configure_pwm3();
__interrupt void pwm_interrupt (void);
#endif /* PWM_H_ */
I would be glad if anyone of you can help me with this issue.
Regards
Haque