Hi TI,
I'm using TMS320F28335.I downoad lib named C2000MCU_IEC60730_4_00_01_00_setup.exe.When opening the lib,there are many ASM files such as STL_march_test.s file under the directory C:..\C2000MCU_IEC60730_4_00_01_00\IEC60730_STL_Library_v4_00_01_00\IEC60730_safety\v4_00_01_00\source\c28x.Can you give me some advice or resources that I can refer to start coding ASM file?
Best regards,
Frank