Part Number: DRV8301-69M-KIT
Other Parts Discussed in Thread: DRV8301, MOTORWARE
Hi all,
I have recently obtained a DRV8301-HC-EVM Rev D InstaSpin Evaluation board second hand from a friend. I have successfully connected to the InstaSpin Universal GUI and am using Proj_Lab13e to read out motor parameters, however I cannot run the motor as the red Fault LED6 on the board is always lit after the InstaSpin Universal GUI begins running. I would like to find out the cause, whether my DRV8301 chip is dead or whether there is another cause.
Some more info: PVDD is supplied with 12V. My ControlCard is an F2806M. I have disconnected the motor and the fault LED is still lit. I have also tried a different motor with no luck.
I have read through the following thread: https://e2e.ti.com/support/applications/motor_drivers/f/38/p/639691/2360751 which suggests the following debug procedure...
"Please try a simple debug procedure:
1) Disconnect the motor
2) Place 12V on the DRV8301 PVDD
3) Set EN_GATE to a logic high
4) Measure the AVDD, DVDD, and GVDD voltages
If the voltages are not ~6.5V, 3.3V, and 10.5V, there is a problem with the DRV8301."
Which C file in the code can I find EN_GATE in? Also where are AVDD DVDD and GVDD voltages found? Should they be measured physically on the board or can I find their value in a register in Code Composer Studio?
Thank you kindly,
Matt