Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Hi,
I am working on an application that needs to use an asynchronous SRAM (Cypress CY62187EV30) to store data using a F2837x controlCard Rev1.3. I configured the EMI1 interface to communicate with it; however, I am having issues with the data I am writing/reading. I am following the "emif1_16bit_asram_cpu01" as a reference and this is not working either.
I configured EM1BA[1] as address 0, and then rest of GPIO's as address 1 and son on. The datasheet states that only EM1BA[1] should be used for a 16 bit interface; however, the example goes on and configures EM1BA[0] as well. Do I need to configure both bits for a 16 bit interface ?
Please let me know if you can help me with this issue.
Thanks,
Gilmer