Part Number: TMS320F28377D
Other Parts Discussed in Thread: TIDM-DELFINO-ETHERCAT, CCSTUDIO
Tool/software: Code Composer Studio
Hello. I'm currently trying to implement EtherCAT communication by using F28377D.
In TI home page, I could find some materials for EtherCAT communication such as evaluation boards, named Launch Pad, and an example software (CCS project) for the board. They are linked in "http://www.ti.com/tool/TIDM-DELFINO-ETHERCAT"
However, I have a problem at importing the example software on CCS. The software has been downloaded on the above link, and its name is “TIDM-DELFINO-ETHERCAT Software (Rev. A) (ZIP, 4498KB), 07 Jun 2017”
The error message is as follows:
“Error: Import failed for project 'pdi_hal_test_app' because its compiler definition is not available. Please install the C2000v15.9 compiler before importing this project - click 'View > CCS App Center' to check if compiler updates are available, or install the compiler manually and register it with CCS through 'Preferences > CCS > Build > Compilers'.”
I have updated the compiler to the latest version (v18.1.1.LTS), but the result was the same. The C2000v15.9 compiler mentioned in the error message, was not found in TI home page.
I tried that under CCS version 6.1.1 and 7.1.0. in Windows 10.
Please, let me know what should I do.
Thanks.