This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377S: SPI hardware circuit/layout guide for TMS320F28377S

Part Number: TMS320F28377S

My customer will plan to use SPI for two TMS320F28377S communication at 50MHz clock speed,

do we have any hardware circuit / layout guide for about 20cm distance design between two TMS320F28377S?

Thanks

  • Hardy,

    When routing high speed signals you should have a continuous ground plane (without breaks or channels) directly above or below the signal trace. Such controlled impedance provides clean current return path to ground.

    Regards,
    PEter