Part Number: TMS320F28035
Other Parts Discussed in Thread: SFRA, CONTROLSUITE
Tool/software: Code Composer Studio
hello sir/madam,
i try to immigrate the SFRA in fixed point 28035 following the guide doc "C2000 Software Frequency Response Analyzer (SFRA) Library & Compensation Designer".
the serial communication is established successfully but when start to sweep, there is no indication the status bar, everything turn to grey and no error appear.
1. i add following code in the background task
if(initializationFlag == 1)
{
SFRA_IQ_INIT(&SFRA1);
initializationFlag = 0;
SFRA1.start = 1;
}
SerialHostComms();
2. i add SerialCommsTimer++ in the 1ms task.
3. add code in the ISR
SFRA_i32Iref = SFRA_IQ_INJECT(SFRA_i32IoutSetSlewed);
SFRA_IQ_COLLECT(&SFRA_i32Iref,&SFRA_i32Fdbk);
then i try to add SFRA_IQ_BACKGROUND(&SFRA1); in the background task which is not mentioned in the use of fixed point SFRA lib but float point SFRA lib.
here always a build error that
undefined first referenced
symbol in file
--------- ----------------
__IQ16log D:/WSP/DSP_WorkSpace/OBC33_LLC_SFRA/build/SFRA_IQ_Lib.lib<SFRA_IQ_BACKGROUND.obj>
my questions are.
1. what's the SFRA_IQ_BACKGROUND(&SFRA1) used for? is it a mandatory for fixed point SFRA lib?
2. how to remove this link error?
3. are there any points i missed making SFRA work?
thank you