Part Number: TMDSHVMTRINSPIN
I am evaluating FAST with an ACI traction-motor application in mind. The motor I'm ultimately wanting to control is a four-pole rated at 600 amps at 96V. I've noted that the typical ADC full scale current for the kit GUI is about 20 with a full scale IQ current of 10.
Do you believe the decreased analog resolution (i.e. 0 to 3.3V for 0 to 600 amps) will still allow FAST to successfully control such a motor?
Do you believe the FAST logic can successfully "identify" such a motor?
Currently working with small motors to understand the technology before scaling up. Just wanting to know such a scale up is possible.